Part Number: AM3352
Yocto/bitbake ends to error messages telling that:
linux-ti-staging-rt_4.4.bb: Failure expanding variable SRCPV
fatal: unable to connect to git.ti.com:
This happens nearly always. Problem has been active several days but not before.
This is highly annoying. Recipe parsing proceeds up to 97% then it stays there for pretty long time then times out.
Is there anything I can do here/should I expect this problem to be solved on TI side (hopefully pretty soon)?
Thanks,
Matti