This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Qt-OpenCV-OpenCL-OpenGL multithreaded

Part Number: AM5728


Hi,

1.Can qt-opencv-opencl-opengl-multithreaded -1.3.3 running on a linux-rt?

2.Is opencv running on A15? Can it be used to DSP?

3.Is philips. Cl running on DSP ? What is the main purpose of this program?

4.If i want to disable one DSP core, which file should be modified?