This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use flash v1.3 for 3517EVM to load bootloader through UART3

Other Parts Discussed in Thread: AM3517, AM3505, AM3703, AM3715, DM3730, DM3725, OMAP3525, OMAP3515, OMAP3530, OMAP3503

I'm using Zoom AM3517 EVM Development kit.

I'm trying to load u-boot.bin through UART3 using Flash V1.3. It is throwing following error. Can any one pls tel me how to go about this this issue.?

Error:

¯ -stdout

¯ -omap 3

¯ -com 1

¯ -t 60

¯ -p CUSTOM_OMAP35XX_BOARD

¯ -2

¯ chip_download SDRAM Z:\svn_folder\lable25\AM35x-OMAP35x-PSP-SDK-03.00.00.05\images\u-boot\am3517\u-boot.bin

¯ Leaving parameter file:temp_script.txt

¯ @temp_script.txt

¯ Looking for device (omap com1)

¯ Please turn off device, then turn it on again

¯ Awaiting ASIC id

¯ Awaiting ASIC id

¯ AsicId items 04

¯ AsicId id 01 05 01 34 30 07 58

¯ AsicId secure_mode 13 02 01 00

¯ AsicId public_id 12 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

¯ AsicId root_key_hash 14 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

¯ Searching 2nd for: CUSTOM_OMAP35XX_BOARD 343007 58 GP

¯ Error no 2nd for: CUSTOM_OMAP35XX_BOARD 343007 58 GP

 

Console program failed, exit code: 2

I did't modify the configuration file. Do I need to any changes in that. if so wat type of changes?

Pls give the link to Flash V1.2, I wanted to try with that once.

Thanks

Sudhee