Part Number: AM5718
Hi,
I want to use Cortex-A15 MPU core to run Linux program and communicate with the Host computer through PCI-E interface. In general, MPU is the Endpoint of PCI-E system, and the Host computer is the Root Complex.
I know that when the MPU is the master device, it needs to compile Linux driver to drive the PCIe slave device. But if the MPU is a slave device, how should I compile the PCIe driver?
I need to compile the PCIe driver as if the MPU were the master device? Or I don't need to compile the PCIe driver, the master device can access to the MPU though the PCIe Controller of AM5718.
Where can I get the example program?
Thank you for your reply.