Hi Sitara support Team,
My customer system used AM3357 is facing the damage of AM3357.
The reason to have AM3357 damaged, he chages from the AM3357
on their system to the new AM3357, it works.
He supposes that it is difficult to have device damaged
without an external stress in the debug use.
So, he finds a point that he is concerned about the cause of damage.
Q. If it accidentally changes the PRU0(1) General-Purpose Outputs Signals
settings on the customer system' source code,
is there any risk of damage such as collision between the output on ARM side
and the output on PRU side?
Best regards,
Kanae