This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 EVMFlash Tool

Other Parts Discussed in Thread: OMAP3530

Can you provide us with a contact name in TI group that develops flashing tools such as EVMFlash?


To flash Micron NAND Flash that we use with OMAP3530 we need a version of the EVMFlash tool that is capable of flashing block 0 with OMAP’s 1-bit ECC engine and blocks 1 thru N with Micron’s on-die 4-bit ECC engine.  We would like to discuss with the tools group the availability of such version or steps required to generate this version.

  • We don't currently have the on-die ECC support built into the Flash tool, but it is coming soon.

    Source code is available and we welcome third-party development efforts.  Some features in Flash have already been developed in this way by the community.  You can join the project and download the code via SVN at this link:  https://gforge.ti.com/gf/project/flash/