Hi Experts:
Our customer use J7 design their cluster system. Compare with their old J6 + MCU ( RH850 ), they meet problem that " last mode" can not implement at J7 system.
J6 + MCU system, MCU power supply 3.3V customer use diode + 2F large capacitor can meet MCU ADC pin probe the 12V drop, story ~200 - 300 Bytes of last mode status to EEPROM at 2ms time windows like attached picture.
Because TDA4x MCU island VDD_MCU_0V85 + VDA_MCU_1V8 + VDD_MCUIO_1V8 + VDD_MCUIO_3V3 all power rail add large capacitor is not reasonable. So I think J7 MCU domain can not meet customer " last mode" function request use the same method. Except period store EEPROM, does we have method to keep MCU island work 2ms to store data to EEPROM when 12V power supply suddenly turn off?
Best Regards!
Han Tao