Part Number: TMDSLCDK138
Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Tool/software: TI C/C++ Compiler
Dear all:
According to this doc. under below:
when I Done the step of picture under below。and rebuild arm application <uart_armv5_omapl138_evmOMAPL138> to generate uart.out file.
was excluted successful under CCS
when if flash uart.bin to NAND by sfh_OMAPL138.exe tool,bootloader is run,but uart application start failed;
BootLoader codes under below:
/******************************************************************************
** Global Variable Definitions
*******************************************************************************/
unsigned int entryPoint = 0xc1080000;
unsigned int DspEntryPoint = 0xc009d000;
int main(void)
{
/* Configures PLL and DDR controller*/
BlPlatformConfig();
UARTPuts("StarterWare ", -1);
UARTPuts(deviceType, -1);
UARTPuts(" Boot Loader\n\r", -1);
/* Copies application from non-volatile flash memory to RAM */
ImageCopy();
UARTPuts("Jumping to StarterWare Application...\r\n\n", -1);
/* Do any post-copy config before leaving boot loader */
BlPlatformConfigPostBoot();
/* Giving control to the application */
appEntry = (void (*)(void)) entryPoint;
UARTPuts("Running arm Application...\r\n\n", -1);
(*appEntry)( );
return 0;
}
Power on and booting, console print like this :
Jumping to StarterWare Application...
Running DSP Application...
Running arm Application...
I want to know how to solve this problem?
Thanks!