This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suggestions for a FS USB (3-Pin Bi-directional) with DM3730.

Other Parts Discussed in Thread: DM3730

I am reviewing the Technical Reference Manual for the DM3730 processor.  I need a Full_Speed USB port and the “MM1..3” ports appear to be a good fit.  I would like to use the port as shown on page 3228 of the technical manual.  I am however having difficulty finding a transceiver that works in this mode, most require ULPI.  

 
--------> mm3_txen_n        -------->   TXEN                                FS/LS USB Peripheral Controller

<--------> mm3_txdat        <-------->   DAT                                3-Pin Bi-Directional
 
<--------> mm3_txse0       <-------->   SE0                                 (Tx = DAT/SE0)

<-------- mm3_rxrcv

<-------- mm3_rxdp

<-------- mm3_rxdm
 

Can you recommend a reference design which utilizes this?

Can you recommend a FS USB Transceiver which is proven to work with the DM processors in this way?

-Tom-