This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

stopped at 'starting kernel'



1. the target hw is our own , the ref.design is from Appro DM368 IPNC sch.

2. we used the Appro's uImage.

·         3. it stopped at 'Starting Kernel .... '.

·           refer below message

---------------------------------------------------------------------

DM36x initialization passed!

TI UBL Version: 1.50

Booting Catalog Boot Loader

BootMode = NAND

Starting NAND Copy...

Valid magicnum, 0xA1ACED66, found in block 0x00000008.

   DONE

Jumping to entry point at 0x81080000.

 

Reset RTC Fail..

DM368_IPNC_UBL_1.0.0

U-Boot 1.3.4 (Apr 20 2010 - 11:42:44) DM368-IPNC-1.0.0

 

I2C:   ready

DRAM:  128 MB

NAND:  NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)

Bad block table found at page 65472, version 0x01

Bad block table found at page 65408, version 0x01

128 MiB

In:    serial

Out:   serial

Err:   serial

ARM Clock :- 432MHz

DDR Clock :- 340MHz

Ethernet PHY: GENERIC @ 0x01

Hit any key to stop autoboot:  0

 

NAND read: device 0 offset 0x700000, size 0xd00000

13631488 bytes read: OK

 

Loading from NAND 128MiB 3,3V 8-bit, offset 0x500000

   Image Name:   Linux-2.6.18_pro500-davinci_IPNC

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    1809680 Bytes =  1.7 MB

   Load Address: 80008000

   Entry Point:  80008000

## Booting kernel from Legacy Image at 80700000 ...

   Image Name:   Linux-2.6.18_pro500-davinci_IPNC

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    1809680 Bytes =  1.7 MB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

 

Starting kernel ...

----------------------------------------------------------------------------------------

4. Difference of two systems only install usb part, vca part and sd card or not.

    => two systems :

- appro’ evm board

- our designed board

 

5. I have checked all power. it’s good

 

6. I tested the ddr memory r/w and the nand flash r/w at diagnostic mode

    => all r/w test is good

 

7. I cannot understand this station.

 Why appro’s evm board operate and doesn't our board operate?

(Same software & Almost similar circuit)