Part Number: AM3359
i am developing a project in AM3359 ice ev2 board, i want to disable the Ethernet and USB from U-boot, since my
project requirements says there is no need of Ethernet and USB
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3359
i am developing a project in AM3359 ice ev2 board, i want to disable the Ethernet and USB from U-boot, since my
project requirements says there is no need of Ethernet and USB
Hi Sreenivas,
Sreenivas Ranganath said:i want to disable the Ethernet and USB from U-boot
Typically you can disable U-Boot features like Ethernet and USB using two methods:
Just doing 1 will usually get you where you need, since disabled nodes won't get probed the related initialization won't be performed. Doing 2 in addition to 1 would only be needed to cut down the size of the SPL and U-Boot executables.
Regards, Andreas