Part Number: 66AK2G12
I succeeded in QSPI boot mode and SDCard boot mode.
It has been confirmed that my DSP source is functioning normally.
Now I installed Linux OS.
I want to load DSP with the same source code in a Linux environment.
My question:
1. Is there any other way to load and run DSP.out other than MPMCL command?
2. If I boot the Linux and load it directly into the CCS, It's will operate normally, But If I load with MPMCL, It doesn't work.
if I try that mpmcl load after mpmcl reset are occurs -104 error msg, but I will load again , they are displayed load success msg.
ex)
:~# mpmcl reset dsp0
reset succeeded
:~# mpmcl load dsp0 thunderDSP.out
load failed (error: -104)
:~# mpmcl load dsp0 thunderDSP.out
load succeeded
I have to load twice every time to get a message of success after reset. Is this relevant to not operating normally?
reference(
source memory configuration
name origin length
---------------------------------------------------------------
MSMCSRAM 0c000000 00100000
L2SRAM 10800000 00100000
DDR3 80000000 60000000
DDR3CODE e0000000 20000000
)
3. If DSP loads normally and runs, I want to debug. Is there any way to place a string in the Linux bash directly from the DSP source, such as printf?
Thanks,
DG