Part Number: TMS320C6678
Hi,
I used two C6678 (A to B) with SRIO 2.5Gbps 2x, and the following problems occurred during initialization:
1. Repeat the power-on operation, and the input error-stopped problem occurs approximately every 2000 times;
2. May I use B to send a maintenance package to A to solve this problem. Is this solution stable?
3. By reading related posts, I find the reasons for the errors are as follows. May I confirm which is, and i want to know the detail about the error.
1) The port0 detected a delineation error. The port received an unaligned /SC/ or /PD/ or undefined code-group
2) The port detected an illegal character
3) A character which is not a part of IDLE1 sequence has occured after link initialization