Hi Sir,
TRM version: J721E DRA829/TDA4VM/AM752x Processors Silicon Revision 1.0
in the OSPI section: 12.3.2.4.8.5 Accessing the SRAM
there is a description as follow
If the OSPI_SRAM_PARTITION_CFG_REG[7-0] ADDR_FLD field is set to 0x00,
then 256 locations are allocated to indirect writes and 1 location to indirect reads.
Q1:what is the locations unit?(byte, half-word, word...)