This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM MCSPI Data I/O for master mode.

Hi TI Support Team

From TRM Table 12-855 and Table 12-856 about MCSPI I/O Signal:

  • Master mode: SPI DATA [0] is output for master mode and SPI DATA  [1] is input for master mode from default config. 

Notes from TRM: Direction depends on MCSPI_CHCONF_0/1/2/3[16] DPE0, MCSPI_CHCONF_0/1/2/3[17] DPE1 and MCSPI_CHCONF_0/1/2/3[18] IS bits

So that is means the SPI D[0] can config as input or output @ mast mode. Is it correct ?

Thanks

Yutai