Other Parts Discussed in Thread: AM3352
rt Number: AM3352
Tool/software: Code Composer Studio
Hi
I have config the EDMA transfer by link mode,and my init code is blow :
int32_t Radar_EDMA_Params_Init(void)
{
EDMA3_DRV_Result result = EDMA3_DRV_SOK;
uint32_t chId1 = EDMA3_DRV_HW_CHANNEL_AD;
uint32_t chId2 = EDMA3_DRV_HW_CHANNEL_FFT;
uint32_t tcc1 = EDMA3_DRV_TCC_ANY;
uint32_t tcc2 = EDMA3_DRV_TCC_ANY;
uint32_t chId_ad[EDMA3_CHANNEL_NUM_AD];
uint32_t chId_FFT[EDMA3_CHANNEL_NUM_FFT];
uint32_t BRCnt = 0;
int srcbidx = 0, desbidx = 0;
int srccidx = 0, descidx = 0;
uint32_t acnt;
uint32_t bcnt;
uint32_t ccnt;
uint16_t i;
uint32_t tmp = 0;
uint8_t fpga_start = 1;
EDMA3_DRV_SyncType syncType = EDMA3_DRV_SYNC_AB;
EDMA3_DRV_PaRAMRegs paramSet = {0,0,0,0,0,0,0,0,0,0,0,0};
/* init AD channel edma*/
acnt = ACNT;
bcnt = BCNT_AD;
ccnt = CCNT;
BRCnt = BCNT_AD;
srcbidx = 0;
desbidx = ACNT;
srccidx = 0;
descidx = ACNT*BCNT_AD;
result = Edma3_CacheInvalidate(dstBuff1, MAX_DEST1_SIZE);
if(result != EDMA3_DRV_SOK)
{
Radar_log("\n Edma3_CacheInvalidate unsuccessful\n");
}
//申请主通道
result = EDMA3_DRV_requestChannel (handle_edma_ad, &chId1, &tcc1,
(EDMA3_RM_EventQueue)0,
&callback1, NULL);
if(result != EDMA3_DRV_SOK)
{
Radar_log("\n EDMA3_DRV_requestChannel failed\n");
}
else
{
paramSet.srcAddr = (uint32_t)(GPMC_ADDRESS+0x0A);
paramSet.destAddr = (uint32_t)(dstBuff1);
paramSet.srcBIdx = srcbidx;
paramSet.destBIdx = desbidx;
paramSet.srcCIdx = srccidx;
paramSet.destCIdx = descidx;
paramSet.aCnt = acnt;
paramSet.bCnt = bcnt;
paramSet.cCnt = ccnt;
paramSet.bCntReload = BRCnt;
//paramSet.linkAddr = 0xFFFFu;
/* Reset opt field first */
paramSet.opt = 0x0u;
/* Src & Dest are in INCR modes */
paramSet.opt &= 0xFFFFFFFCu;
/* Program the TCC */
paramSet.opt |= ((tcc1 << OPT_TCC_SHIFT) & OPT_TCC_MASK);
/* Enable Intermediate & Final transfer completion interrupt */
paramSet.opt |= (1 << OPT_ITCINTEN_SHIFT);
paramSet.opt |= (1 << OPT_TCINTEN_SHIFT);
/* AB Sync Transfer Mode */
paramSet.opt |= (1 << OPT_SYNCDIM_SHIFT);
/* Now, write the PaRAM Set. */
result = EDMA3_DRV_setPaRAM (handle_edma_ad, chId1, ¶mSet);
if(result != EDMA3_DRV_SOK)
{
Radar_log("\n EDMA3_DRV_setPaRAM failed result is %d\r\n\n",result);
}
else
{
for(i = 0; i < EDMA3_CHANNEL_NUM_AD; i++)
{
chId_ad[i] = EDMA3_DRV_LINK_CHANNEL;
result = EDMA3_DRV_requestChannel (handle_edma_ad, &chId_ad[i], NULL,
(EDMA3_RM_EventQueue)0,
&callback1, NULL);
if(result != EDMA3_DRV_SOK)
{
Radar_log("\n EDMA3_DRV_requestChannel AD %d failed result is %d\r\n\n",i,result);
}
else
{
if(i < (EDMA3_CHANNEL_NUM_AD - 1))
{
paramSet.destAddr = (uint32_t)(dstBuff1+EDMA_AD_SIZE*2*(i+1));
}
else
{
paramSet.destAddr = (uint32_t)(dstBuff1);
}
result = EDMA3_DRV_setPaRAM (handle_edma_ad, chId_ad[i], ¶mSet);
if(result != EDMA3_DRV_SOK)
{
Radar_log("\n EDMA3_DRV_setPaRAM link channel parames AD %d failed result is %d\r\n\n",i,result);
}
}
}
}
if(result == EDMA3_DRV_SOK)
{
result = EDMA3_DRV_linkChannel(handle_edma_ad, chId1, chId_ad[0]);
for (i = 0; i < EDMA3_CHANNEL_NUM_AD; i++)
{
result = EDMA3_DRV_linkChannel(handle_edma_ad, chId_ad[i], chId_ad[(i+1)%32]);
}
}
//event 22 is enabled
//WR_MEM_32(EDMA_REG_BASE_ADDR+EDMA_REG_EESR_OFFSET, 1<<EDMA3_DRV_HW_CHANNEL_AD);
if(result == EDMA3_DRV_SOK)
{
result = EDMA3_DRV_enableTransfer(handle_edma_ad,chId1,EDMA3_DRV_TRIG_MODE_EVENT);
if(result == EDMA3_DRV_SOK)
{
Radar_log("\n EDMA3_DRV_enableTransfer successful\r\n");
}
}
if(result != EDMA3_DRV_SOK)
{
Radar_log("\n EDMA3_DRV_enableTransfer failed chId1 is %d result is %d\r\n",chId1,result);
}
Radar_gpmc_write(&fpga_start, 1,0x16);// start fpga sampling data
}
return result;
}
the PDK version is pdk_am335x_1_0_13 and the EDMA3 LLD version is edma3_lld_2_12_05_30C.
my issue is :I can only get the write at the first 32 transfer,I have set 32 link channels.
No new data was obtained in the second round。
please help me resolve this issue.
BR!