Hi,
I am using BSP_WINCE_ARM_A8_01_00_00 on AM3517, there is only one named "SMSC91181" and one named "EMAC1" ethernet connections appeared in WinCE OS, but the LAN9311 on AM3517 EVM should have two ports can be used.
Does there any setting need to modify to support two ports of LAN9311?
Another question, even the ethernet cable has not connected to the port, it will keep the status of icon in connection(the icon at the the right-lower corner doesn't become disconnection). This were happened on both "EMAC1" and "SMSC91181" ports. Could someone help to check this?
Thank you.
Indy