Dear Ti support team
I need boot argument value for args_mmc if using DAN-PRP on TMDSICE3359
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Ti support team
I need boot argument value for args_mmc if using DAN-PRP on TMDSICE3359
Hi,
Please provide complete details of your use case. Which SDK you are using - Linux or RTOS, what version, etc....
Hi Biser,
I am working on PROCESSOR-SDK-LINUX-AM335X 06_01_00_08 for PRP on TMDSICE3359.
There is some typing mistake in SDK documentation of Getting Started Guide
SoC | ID | if number | ICSS TRM reference |
---|---|---|---|
AM3 | 0 | eth0/1 | PRU-ICSS |
AM4 | 0 | eth1/2 | PRU-ICSS0 |
AM571 | 1 | eth2/3 | PRU-ICSS1 |
AM571 | 2 | eth4/5 | PRU-ICSS2 |
AM572/4 | 2 | eth2/3 | PRU-ICSS2 |
K2G | 0 | eth1/2 | PRU-ICSS0 |
K2G | 1 | eth3/4 | PRU-ICSS1 |
When i replace this PRU-ICSS to PRU-ICSS0 in args_mmc boot variable then offload firmware type is selected for PRP mose.
Thank for Reply
Have a nice Day
Part Number: TMDSICE3359
Dear Biser,
During testing of PRP based on PROCESSOR-SDK-LINUX-AM335X 06_01_00_08 using TMDSICE3359, It is observed that packet latency is more than 1ms for ping test.
what is the issue & how can i resolve this.
Thanks
Sachin Barkul
Hello Sachin,
We assume that the ping test latency is the same question as the post PRP Latency Issue. If so, we will leave this thread about boot variables, and do the latency discussion on the other thread.
Regards,
Nick
Hi Nick,
Ok no issue, we discussed on PRP Latency Issue Thread link in last message & close this thread now.