This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to connect ADS1606 EVM to tmdxoskl138

Other Parts Discussed in Thread: ADS1606, OMAP-L138, ADS1605

Original Thread : http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/p/12173/300324.aspx#300324

 

Hello Champs,

 

Can the ADS1606 EVM fit into the OMAP-L138 EVM from Logic PD? If not what are the options to test the 2 connected via uPP?

 

Can the 5-6K card be used?

 

Best Regards

Feroz

 

  • I split this thread as the original one was already marked answered.  Please do not post on top of it, but rather reference the thread if you have a follow up question and post a new one.

    That said, the original post answers 2 of the 3 questions already.

    K Md Feroz Irfan said:

    Can the ADS1606 EVM fit into the OMAP-L138 EVM from Logic PD?

    No, answered in Mariana's response.

     

    K Md Feroz Irfan said:

    If not what are the options to test the 2 connected via uPP?

    In order to connect the 2 EVMs, you would need to create (design and build) an interposer board that has appropriate mating connectors for both EVMs and board traces and possibly conditioning logic to connect them.

    Secondly, the ADS1606 has an internal FIFO and an asynchronous SRAM-like bus interface anyway.  You would likely connect it to the asynchronous EMIF of a Processor and not the UPP.

     

    K Md Feroz Irfan said:
     

    Can the 5-6K card be used?

    No.  Mariana's response indicated the EVMs are not natively compatible.  Specifically she says:

    The OMAP-L138 EVM does not have the 80-pin conector, so you would need to do a lot of adaptations.

  • Hello Brandon,

     

     

    Can ADS1605EVM be interfaced to the  OMAP-L138 EVM via uPP connector ?

     

    Any ref designs/photos on the options you mentioned will be of great help 

     

    Please let me know.

     

    Thanks!

     

    Best Regards

    Regards

  • K Md Feroz Irfan said:
    Can ADS1605EVM be interfaced to the  OMAP-L138 EVM via uPP connector ?

    This is the same issue.  No, the ADS1605/ADS1606 EVM can not be interfaced to the OMAP-L138 EVM in this way.  I thought that was clear.

     

    K Md Feroz Irfan said:

    Any ref designs/photos on the options you mentioned will be of great help 

    I didn't mention any reference designs.  I indicated "you would have to create", ie. this is something you are another company would need to design and build yourself.  Nothing currently exists to do this.