Hi Champs:
We are porting the TI DP82825 Phy by using the patch onto DP83822.
Can you guide us where is to open the DP83822 on the Sitara SDK?
I have check the 5.02.10 / 5.03 , there is no DP83822 menuconfig..
BR Rio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI .
I can add the menu config item for DP82825 in the kernel menuconfig now.
But, I also need to add it onto the uboot.
Since our SDK uboot only has the DP83867 in the uboot, I don't have the DP83825 drvier for uboot.
I know there is DP83822/825 kernel driver like this: https://lkml.org/lkml/2019/3/19/768
But the driver for uboot vs Kernel is different. See the attached DP83867 driver,
So, where is the DP83825 uboot Phy driver?
/*
* Driver for the Texas Instruments DP83867 PHY
*
* Copyright (C) 2015 Texas Instruments Inc.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License as published by
* the Free Software Foundation; either version 2 of the License.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*/
#include <linux/ethtool.h>
#include <linux/kernel.h>
#include <linux/mii.h>
#include <linux/module.h>
#include <linux/of.h>
#include <linux/phy.h>
#include <dt-bindings/net/ti-dp83867.h>
#define DP83867_PHY_ID 0x2000a231
#define DP83867_DEVADDR 0x1f
#define MII_DP83867_PHYCTRL 0x10
#define MII_DP83867_MICR 0x12
#define MII_DP83867_ISR 0x13
#define DP83867_CTRL 0x1f
#define DP83867_CFG3 0x1e
/* Extended Registers */
/* TBD register name to be available in a new revision of the TRM */
#define DP83867_FLD_THRESH 0x002E
#define DP83867_CFG4 0x0031
#define DP83867_RGMIICTL 0x0032
#define DP83867_STRAP_STS1 0x006E
#define DP83867_STRAP_STS2 0x006F
#define DP83867_RGMIIDCTL 0x0086
#define DP83867_IO_MUX_CFG 0x0170
#define DP83867_SW_RESET BIT(15)
#define DP83867_SW_RESTART BIT(14)
#define STRAP_STS2_FLD_MASK BIT(10)
/* MICR Interrupt bits */
#define MII_DP83867_MICR_AN_ERR_INT_EN BIT(15)
#define MII_DP83867_MICR_SPEED_CHNG_INT_EN BIT(14)
#define MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN BIT(13)
#define MII_DP83867_MICR_PAGE_RXD_INT_EN BIT(12)
#define MII_DP83867_MICR_AUTONEG_COMP_INT_EN BIT(11)
#define MII_DP83867_MICR_LINK_STS_CHNG_INT_EN BIT(10)
#define MII_DP83867_MICR_FALSE_CARRIER_INT_EN BIT(8)
#define MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN BIT(4)
#define MII_DP83867_MICR_WOL_INT_EN BIT(3)
#define MII_DP83867_MICR_XGMII_ERR_INT_EN BIT(2)
#define MII_DP83867_MICR_POL_CHNG_INT_EN BIT(1)
#define MII_DP83867_MICR_JABBER_INT_EN BIT(0)
/* RGMIICTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_EN BIT(1)
#define DP83867_RGMII_RX_CLK_DELAY_EN BIT(0)
/* STRAP_STS1 bits */
#define DP83867_STRAP_STS1_RESERVED BIT(11)
/* PHY CTRL bits */
#define DP83867_PHYCR_FIFO_DEPTH_SHIFT 14
#define DP83867_PHYCR_FIFO_DEPTH_MASK (3 << 14)
#define DP83867_PHYCR_RESERVED_MASK BIT(11)
/* RGMIIDCTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_SHIFT 4
/* IO_MUX_CFG bits */
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL 0x1f
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_MAX 0x0
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_MIN 0x1f
/* CFG4 bits */
#define DP83867_CFG4_PORT_MIRROR_EN BIT(0)
enum {
DP83867_PORT_MIRROING_KEEP,
DP83867_PORT_MIRROING_EN,
DP83867_PORT_MIRROING_DIS,
};
struct dp83867_private {
int rx_id_delay;
int tx_id_delay;
int fifo_depth;
int io_impedance;
int port_mirroring;
bool rxctrl_strap_quirk;
};
static int dp83867_ack_interrupt(struct phy_device *phydev)
{
int err = phy_read(phydev, MII_DP83867_ISR);
if (err < 0)
return err;
return 0;
}
static int dp83867_config_intr(struct phy_device *phydev)
{
int micr_status;
if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
micr_status = phy_read(phydev, MII_DP83867_MICR);
if (micr_status < 0)
return micr_status;
micr_status |=
(MII_DP83867_MICR_AN_ERR_INT_EN |
MII_DP83867_MICR_SPEED_CHNG_INT_EN |
MII_DP83867_MICR_AUTONEG_COMP_INT_EN |
MII_DP83867_MICR_LINK_STS_CHNG_INT_EN |
MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN |
MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN);
return phy_write(phydev, MII_DP83867_MICR, micr_status);
}
micr_status = 0x0;
return phy_write(phydev, MII_DP83867_MICR, micr_status);
}
static int dp83867_config_port_mirroring(struct phy_device *phydev)
{
struct dp83867_private *dp83867 =
(struct dp83867_private *)phydev->priv;
u16 val;
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4);
if (dp83867->port_mirroring == DP83867_PORT_MIRROING_EN)
val |= DP83867_CFG4_PORT_MIRROR_EN;
else
val &= ~DP83867_CFG4_PORT_MIRROR_EN;
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4, val);
return 0;
}
#ifdef CONFIG_OF_MDIO
static int dp83867_of_init(struct phy_device *phydev)
{
struct dp83867_private *dp83867 = phydev->priv;
struct device *dev = &phydev->mdio.dev;
struct device_node *of_node = dev->of_node;
int ret;
if (!of_node)
return -ENODEV;
dp83867->io_impedance = -EINVAL;
/* Optional configuration */
if (of_property_read_bool(of_node, "ti,max-output-impedance"))
dp83867->io_impedance = DP83867_IO_MUX_CFG_IO_IMPEDANCE_MAX;
else if (of_property_read_bool(of_node, "ti,min-output-impedance"))
dp83867->io_impedance = DP83867_IO_MUX_CFG_IO_IMPEDANCE_MIN;
dp83867->rxctrl_strap_quirk = of_property_read_bool(of_node,
"ti,dp83867-rxctrl-strap-quirk");
ret = of_property_read_u32(of_node, "ti,rx-internal-delay",
&dp83867->rx_id_delay);
if (ret &&
(phydev->interface == PHY_INTERFACE_MODE_RGMII_ID ||
phydev->interface == PHY_INTERFACE_MODE_RGMII_RXID))
return ret;
ret = of_property_read_u32(of_node, "ti,tx-internal-delay",
&dp83867->tx_id_delay);
if (ret &&
(phydev->interface == PHY_INTERFACE_MODE_RGMII_ID ||
phydev->interface == PHY_INTERFACE_MODE_RGMII_TXID))
return ret;
if (of_property_read_bool(of_node, "enet-phy-lane-swap"))
dp83867->port_mirroring = DP83867_PORT_MIRROING_EN;
if (of_property_read_bool(of_node, "enet-phy-lane-no-swap"))
dp83867->port_mirroring = DP83867_PORT_MIRROING_DIS;
return of_property_read_u32(of_node, "ti,fifo-depth",
&dp83867->fifo_depth);
}
#else
static int dp83867_of_init(struct phy_device *phydev)
{
return 0;
}
#endif /* CONFIG_OF_MDIO */
static int dp83867_config_init(struct phy_device *phydev)
{
struct dp83867_private *dp83867;
int ret, val, bs;
u16 delay;
if (!phydev->priv) {
dp83867 = devm_kzalloc(&phydev->mdio.dev, sizeof(*dp83867),
GFP_KERNEL);
if (!dp83867)
return -ENOMEM;
phydev->priv = dp83867;
ret = dp83867_of_init(phydev);
if (ret)
return ret;
} else {
dp83867 = (struct dp83867_private *)phydev->priv;
}
/* RX_DV/RX_CTRL strapped in mode 1 or mode 2 workaround */
if (dp83867->rxctrl_strap_quirk) {
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4);
val &= ~BIT(7);
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4, val);
}
/* When the Phy is strapped to enable Fast Link Drop (FLD) feature,
* the detect threshold value becomes 0x2 in bit 2:0 instead of 0x1
* as in non strapped case. This causes the phy link to be unstable.
* As a workaround, write a value of 0x1 in this bit field if
* bit 10 of DP83867_STRAP_STS2 is set (enable FLD).
*/
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_STRAP_STS2);
if (val & STRAP_STS2_FLD_MASK) {
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_FLD_THRESH);
val &= ~0x7;
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_FLD_THRESH,
val | 0x1);
}
if (phy_interface_is_rgmii(phydev)) {
val = phy_read(phydev, MII_DP83867_PHYCTRL);
if (val < 0)
return val;
val &= ~DP83867_PHYCR_FIFO_DEPTH_MASK;
val |= (dp83867->fifo_depth << DP83867_PHYCR_FIFO_DEPTH_SHIFT);
/* The code below checks if "port mirroring" N/A MODE4 has been
* enabled during power on bootstrap.
*
* Such N/A mode enabled by mistake can put PHY IC in some
* internal testing mode and disable RGMII transmission.
*
* In this particular case one needs to check STRAP_STS1
* register's bit 11 (marked as RESERVED).
*/
bs = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_STRAP_STS1);
if (bs & DP83867_STRAP_STS1_RESERVED)
val &= ~DP83867_PHYCR_RESERVED_MASK;
ret = phy_write(phydev, MII_DP83867_PHYCTRL, val);
if (ret)
return ret;
}
if ((phydev->interface >= PHY_INTERFACE_MODE_RGMII_ID) &&
(phydev->interface <= PHY_INTERFACE_MODE_RGMII_RXID)) {
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIICTL);
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_ID)
val |= (DP83867_RGMII_TX_CLK_DELAY_EN | DP83867_RGMII_RX_CLK_DELAY_EN);
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_TXID)
val |= DP83867_RGMII_TX_CLK_DELAY_EN;
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_RXID)
val |= DP83867_RGMII_RX_CLK_DELAY_EN;
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIICTL, val);
delay = (dp83867->rx_id_delay |
(dp83867->tx_id_delay << DP83867_RGMII_TX_CLK_DELAY_SHIFT));
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIIDCTL,
delay);
if (dp83867->io_impedance >= 0) {
val = phy_read_mmd(phydev, DP83867_DEVADDR,
DP83867_IO_MUX_CFG);
val &= ~DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL;
val |= dp83867->io_impedance &
DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL;
phy_write_mmd(phydev, DP83867_DEVADDR,
DP83867_IO_MUX_CFG, val);
}
}
/* Enable Interrupt output INT_OE in CFG3 register */
if (phy_interrupt_is_valid(phydev)) {
val = phy_read(phydev, DP83867_CFG3);
val |= BIT(7);
phy_write(phydev, DP83867_CFG3, val);
}
if (dp83867->port_mirroring != DP83867_PORT_MIRROING_KEEP)
dp83867_config_port_mirroring(phydev);
return 0;
}
static int dp83867_phy_reset(struct phy_device *phydev)
{
int err;
err = phy_write(phydev, DP83867_CTRL, DP83867_SW_RESET);
if (err < 0)
return err;
return dp83867_config_init(phydev);
}
static struct phy_driver dp83867_driver[] = {
{
.phy_id = DP83867_PHY_ID,
.phy_id_mask = 0xfffffff0,
.name = "TI DP83867",
.features = PHY_GBIT_FEATURES,
.flags = PHY_HAS_INTERRUPT,
.config_init = dp83867_config_init,
.soft_reset = dp83867_phy_reset,
/* IRQ related */
.ack_interrupt = dp83867_ack_interrupt,
.config_intr = dp83867_config_intr,
.config_aneg = genphy_config_aneg,
.read_status = genphy_read_status,
.suspend = genphy_suspend,
.resume = genphy_resume,
},
};
module_phy_driver(dp83867_driver);
static struct mdio_device_id __maybe_unused dp83867_tbl[] = {
{ DP83867_PHY_ID, 0xfffffff0 },
{ }
};
MODULE_DEVICE_TABLE(mdio, dp83867_tbl);
MODULE_DESCRIPTION("Texas Instruments DP83867 PHY driver");
MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com");
MODULE_LICENSE("GPL");
/*
* TI PHY drivers
*
* SPDX-License-Identifier: GPL-2.0
*
*/
#include <common.h>
#include <phy.h>
#include <linux/compat.h>
#include <malloc.h>
#include <dm.h>
#include <dt-bindings/net/ti-dp83867.h>
/* TI DP83867 */
#define DP83867_DEVADDR 0x1f
#define MII_DP83867_PHYCTRL 0x10
#define MII_DP83867_MICR 0x12
#define MII_DP83867_CFG2 0x14
#define MII_DP83867_BISCR 0x16
#define DP83867_CTRL 0x1f
/* Extended Registers */
#define DP83867_CFG4 0x0031
#define DP83867_RGMIICTL 0x0032
#define DP83867_RGMIIDCTL 0x0086
#define DP83867_IO_MUX_CFG 0x0170
#define DP83867_SW_RESET BIT(15)
#define DP83867_SW_RESTART BIT(14)
/* MICR Interrupt bits */
#define MII_DP83867_MICR_AN_ERR_INT_EN BIT(15)
#define MII_DP83867_MICR_SPEED_CHNG_INT_EN BIT(14)
#define MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN BIT(13)
#define MII_DP83867_MICR_PAGE_RXD_INT_EN BIT(12)
#define MII_DP83867_MICR_AUTONEG_COMP_INT_EN BIT(11)
#define MII_DP83867_MICR_LINK_STS_CHNG_INT_EN BIT(10)
#define MII_DP83867_MICR_FALSE_CARRIER_INT_EN BIT(8)
#define MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN BIT(4)
#define MII_DP83867_MICR_WOL_INT_EN BIT(3)
#define MII_DP83867_MICR_XGMII_ERR_INT_EN BIT(2)
#define MII_DP83867_MICR_POL_CHNG_INT_EN BIT(1)
#define MII_DP83867_MICR_JABBER_INT_EN BIT(0)
/* RGMIICTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_EN BIT(1)
#define DP83867_RGMII_RX_CLK_DELAY_EN BIT(0)
/* PHY CTRL bits */
#define DP83867_PHYCR_FIFO_DEPTH_SHIFT 14
#define DP83867_MDI_CROSSOVER 5
#define DP83867_MDI_CROSSOVER_AUTO 2
#define DP83867_MDI_CROSSOVER_MDIX 2
#define DP83867_PHYCTRL_SGMIIEN 0x0800
#define DP83867_PHYCTRL_RXFIFO_SHIFT 12
#define DP83867_PHYCTRL_TXFIFO_SHIFT 14
/* RGMIIDCTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_SHIFT 4
/* CFG2 bits */
#define MII_DP83867_CFG2_SPEEDOPT_10EN 0x0040
#define MII_DP83867_CFG2_SGMII_AUTONEGEN 0x0080
#define MII_DP83867_CFG2_SPEEDOPT_ENH 0x0100
#define MII_DP83867_CFG2_SPEEDOPT_CNT 0x0800
#define MII_DP83867_CFG2_SPEEDOPT_INTLOW 0x2000
#define MII_DP83867_CFG2_MASK 0x003F
#define MII_MMD_CTRL 0x0d /* MMD Access Control Register */
#define MII_MMD_DATA 0x0e /* MMD Access Data Register */
/* MMD Access Control register fields */
#define MII_MMD_CTRL_DEVAD_MASK 0x1f /* Mask MMD DEVAD*/
#define MII_MMD_CTRL_ADDR 0x0000 /* Address */
#define MII_MMD_CTRL_NOINCR 0x4000 /* no post increment */
#define MII_MMD_CTRL_INCR_RDWT 0x8000 /* post increment on reads & writes */
#define MII_MMD_CTRL_INCR_ON_WT 0xC000 /* post increment on writes only */
/* User setting - can be taken from DTS */
#define DEFAULT_RX_ID_DELAY DP83867_RGMIIDCTL_2_25_NS
#define DEFAULT_TX_ID_DELAY DP83867_RGMIIDCTL_2_75_NS
#define DEFAULT_FIFO_DEPTH DP83867_PHYCR_FIFO_DEPTH_4_B_NIB
/* IO_MUX_CFG bits */
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL 0x1f
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_MAX 0x0
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_MIN 0x1f
struct dp83867_private {
int rx_id_delay;
int tx_id_delay;
int fifo_depth;
int io_impedance;
bool rxctrl_strap_quirk;
};
/**
* phy_read_mmd_indirect - reads data from the MMD registers
* @phydev: The PHY device bus
* @prtad: MMD Address
* @devad: MMD DEVAD
* @addr: PHY address on the MII bus
*
* Description: it reads data from the MMD registers (clause 22 to access to
* clause 45) of the specified phy address.
* To read these registers we have:
* 1) Write reg 13 // DEVAD
* 2) Write reg 14 // MMD Address
* 3) Write reg 13 // MMD Data Command for MMD DEVAD
* 3) Read reg 14 // Read MMD data
*/
int phy_read_mmd_indirect(struct phy_device *phydev, int prtad,
int devad, int addr)
{
int value = -1;
/* Write the desired MMD Devad */
phy_write(phydev, addr, MII_MMD_CTRL, devad);
/* Write the desired MMD register address */
phy_write(phydev, addr, MII_MMD_DATA, prtad);
/* Select the Function : DATA with no post increment */
phy_write(phydev, addr, MII_MMD_CTRL, (devad | MII_MMD_CTRL_NOINCR));
/* Read the content of the MMD's selected register */
value = phy_read(phydev, addr, MII_MMD_DATA);
return value;
}
/**
* phy_write_mmd_indirect - writes data to the MMD registers
* @phydev: The PHY device
* @prtad: MMD Address
* @devad: MMD DEVAD
* @addr: PHY address on the MII bus
* @data: data to write in the MMD register
*
* Description: Write data from the MMD registers of the specified
* phy address.
* To write these registers we have:
* 1) Write reg 13 // DEVAD
* 2) Write reg 14 // MMD Address
* 3) Write reg 13 // MMD Data Command for MMD DEVAD
* 3) Write reg 14 // Write MMD data
*/
void phy_write_mmd_indirect(struct phy_device *phydev, int prtad,
int devad, int addr, u32 data)
{
/* Write the desired MMD Devad */
phy_write(phydev, addr, MII_MMD_CTRL, devad);
/* Write the desired MMD register address */
phy_write(phydev, addr, MII_MMD_DATA, prtad);
/* Select the Function : DATA with no post increment */
phy_write(phydev, addr, MII_MMD_CTRL, (devad | MII_MMD_CTRL_NOINCR));
/* Write the data into MMD's selected register */
phy_write(phydev, addr, MII_MMD_DATA, data);
}
#if defined(CONFIG_DM_ETH)
/**
* dp83867_data_init - Convenience function for setting PHY specific data
*
* @phydev: the phy_device struct
*/
static int dp83867_of_init(struct phy_device *phydev)
{
struct dp83867_private *dp83867 = phydev->priv;
ofnode node;
node = phy_get_ofnode(phydev);
if (!ofnode_valid(node))
return -EINVAL;
if (ofnode_read_bool(node, "ti,max-output-impedance"))
dp83867->io_impedance = DP83867_IO_MUX_CFG_IO_IMPEDANCE_MAX;
else if (ofnode_read_bool(node, "ti,min-output-impedance"))
dp83867->io_impedance = DP83867_IO_MUX_CFG_IO_IMPEDANCE_MIN;
else
dp83867->io_impedance = -EINVAL;
if (ofnode_read_bool(node, "ti,dp83867-rxctrl-strap-quirk"))
dp83867->rxctrl_strap_quirk = true;
dp83867->rx_id_delay = ofnode_read_u32_default(
node, "ti,rx-internal-delay", -1);
dp83867->tx_id_delay = ofnode_read_u32_default(
node, "ti,tx-internal-delay", -1);
dp83867->fifo_depth = ofnode_read_u32_default(
node, "ti,fifo-depth", -1);
return 0;
}
#else
static int dp83867_of_init(struct phy_device *phydev)
{
struct dp83867_private *dp83867 = phydev->priv;
dp83867->rx_id_delay = DEFAULT_RX_ID_DELAY;
dp83867->tx_id_delay = DEFAULT_TX_ID_DELAY;
dp83867->fifo_depth = DEFAULT_FIFO_DEPTH;
dp83867->io_impedance = -EINVAL;
return 0;
}
#endif
static int dp83867_config(struct phy_device *phydev)
{
struct dp83867_private *dp83867;
unsigned int val, delay, cfg2;
int ret;
if (!phydev->priv) {
dp83867 = kzalloc(sizeof(*dp83867), GFP_KERNEL);
if (!dp83867)
return -ENOMEM;
phydev->priv = dp83867;
ret = dp83867_of_init(phydev);
if (ret)
goto err_out;
} else {
dp83867 = (struct dp83867_private *)phydev->priv;
}
/* Restart the PHY. */
val = phy_read(phydev, MDIO_DEVAD_NONE, DP83867_CTRL);
phy_write(phydev, MDIO_DEVAD_NONE, DP83867_CTRL,
val | DP83867_SW_RESTART);
/* Mode 1 or 2 workaround */
if (dp83867->rxctrl_strap_quirk) {
val = phy_read_mmd_indirect(phydev, DP83867_CFG4,
DP83867_DEVADDR, phydev->addr);
val &= ~BIT(7);
phy_write_mmd_indirect(phydev, DP83867_CFG4,
DP83867_DEVADDR, phydev->addr, val);
}
if (phy_interface_is_rgmii(phydev)) {
ret = phy_write(phydev, MDIO_DEVAD_NONE, MII_DP83867_PHYCTRL,
(DP83867_MDI_CROSSOVER_AUTO << DP83867_MDI_CROSSOVER) |
(dp83867->fifo_depth << DP83867_PHYCR_FIFO_DEPTH_SHIFT));
if (ret)
goto err_out;
} else if (phy_interface_is_sgmii(phydev)) {
phy_write(phydev, MDIO_DEVAD_NONE, MII_BMCR,
(BMCR_ANENABLE | BMCR_FULLDPLX | BMCR_SPEED1000));
cfg2 = phy_read(phydev, phydev->addr, MII_DP83867_CFG2);
cfg2 &= MII_DP83867_CFG2_MASK;
cfg2 |= (MII_DP83867_CFG2_SPEEDOPT_10EN |
MII_DP83867_CFG2_SGMII_AUTONEGEN |
MII_DP83867_CFG2_SPEEDOPT_ENH |
MII_DP83867_CFG2_SPEEDOPT_CNT |
MII_DP83867_CFG2_SPEEDOPT_INTLOW);
phy_write(phydev, MDIO_DEVAD_NONE, MII_DP83867_CFG2, cfg2);
phy_write_mmd_indirect(phydev, DP83867_RGMIICTL,
DP83867_DEVADDR, phydev->addr, 0x0);
phy_write(phydev, MDIO_DEVAD_NONE, MII_DP83867_PHYCTRL,
DP83867_PHYCTRL_SGMIIEN |
(DP83867_MDI_CROSSOVER_MDIX <<
DP83867_MDI_CROSSOVER) |
(dp83867->fifo_depth << DP83867_PHYCTRL_RXFIFO_SHIFT) |
(dp83867->fifo_depth << DP83867_PHYCTRL_TXFIFO_SHIFT));
phy_write(phydev, MDIO_DEVAD_NONE, MII_DP83867_BISCR, 0x0);
}
if (phy_interface_is_rgmii(phydev)) {
val = phy_read_mmd_indirect(phydev, DP83867_RGMIICTL,
DP83867_DEVADDR, phydev->addr);
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_ID)
val |= (DP83867_RGMII_TX_CLK_DELAY_EN |
DP83867_RGMII_RX_CLK_DELAY_EN);
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_TXID)
val |= DP83867_RGMII_TX_CLK_DELAY_EN;
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_RXID)
val |= DP83867_RGMII_RX_CLK_DELAY_EN;
phy_write_mmd_indirect(phydev, DP83867_RGMIICTL,
DP83867_DEVADDR, phydev->addr, val);
delay = (dp83867->rx_id_delay |
(dp83867->tx_id_delay << DP83867_RGMII_TX_CLK_DELAY_SHIFT));
phy_write_mmd_indirect(phydev, DP83867_RGMIIDCTL,
DP83867_DEVADDR, phydev->addr, delay);
if (dp83867->io_impedance >= 0) {
val = phy_read_mmd_indirect(phydev,
DP83867_IO_MUX_CFG,
DP83867_DEVADDR,
phydev->addr);
val &= ~DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL;
val |= dp83867->io_impedance &
DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL;
phy_write_mmd_indirect(phydev, DP83867_IO_MUX_CFG,
DP83867_DEVADDR, phydev->addr,
val);
}
}
genphy_config_aneg(phydev);
return 0;
err_out:
kfree(dp83867);
return ret;
}
static struct phy_driver DP83867_driver = {
.name = "TI DP83867",
.uid = 0x2000a231,
.mask = 0xfffffff0,
.features = PHY_GBIT_FEATURES,
.config = &dp83867_config,
.startup = &genphy_startup,
.shutdown = &genphy_shutdown,
};
int phy_ti_init(void)
{
phy_register(&DP83867_driver);
return 0;
}
BR Rio
Hi Rio,
That is correct, currently there is not support for the dp83825 PHY at this time in U-boot in the SDK, just the 83867.
Best Regards,
Schuyler