Part Number: AM3352
I am using a 24MHz crystal for OSC0 and have connected the circuit as shown in the AM3352 Datasheet (SPRS717K) Figure 6-9. My crystal complies with the requirements of Table 6-2 i.e
CL = 18pF
Cshunt = 5pF
ESR = 40R
Drive level = 500uW max
When I measure the crystal drive level it is >600uW so I need to add the optional resistor Rd with a value of 120R to reduce it. The effective ESR of my crystal is now 160R. My question is, could this value of ESR reduce the gain margin and prevent the oscillator starting? Is it the case that, to ensure sufficient gain margin to guarantee oscillation, my effective ESR (160R) must be less than the oscillator worst case negative resistance (144R) specified in Table 6-2?
Many thanks in advance for any assistance,
Graham