Part Number: AM6548
Other Parts Discussed in Thread: TLV320AIC3106
Hello TI Team,
We have a custom platform which uses AM6548 SOC which runs Android Pie that need to supports audio over HDMI and Headphone Out.
We are using TLV320AIC3X Codec to implement Headphone functionality and Sil9022 HDMI Transmitter for HDMI Audio. MCASP0 and MCASP2 were used for AIC3X codec and Sil022 HDMI Transmitter respectively.
From software side(Adroid Pie) we are successful to recreate sound card entries for TLV320AIC3X Codec and HDMI Transmitter.
console:/ # cat proc/asound/cards
0 [HDMI ]: HDMI - HDMI
HDMI
1 [AM65xGPEVM ]: AM65x-GPEVM - AM65x-GPEVM
AM65x-GPEVM
The below are the device tree entries for the two sound devices:
sound@0 {
compatible = "simple-audio-card";
simple-audio-card,name = "AM65x-GPEVM";
simple-audio-card,widgets =
"Headphone", "Headphone Jack",
"Line", "Line In";
simple-audio-card,routing =
"Headphone Jack", "HPLOUT",
"Headphone Jack", "HPROUT",
"LINE1L", "Line In",
"LINE1R", "Line In";
simple-audio-card,format = "dsp_b";
simple-audio-card,bitclock-master = <&sound_master>;
simple-audio-card,frame-master = <&sound_master>;
simple-audio-card,bitclock-inversion;
simple-audio-card,cpu {
sound-dai = <&mcasp0>;
};
sound_master: simple-audio-card,codec {
sound-dai = <&tlv320aic3106>;
system-clock-frequency = <12000000>;
};
};
sound@1 {
compatible = "simple-audio-card";
simple-audio-card,name = "HDMI";
simple-audio-card,format = "i2s";
simple-audio-card,bitclock-inversion;
simple-audio-card,bitclock-master = <&hdmi_dailink_master>;
simple-audio-card,frame-master = <&hdmi_dailink_master>;
hdmi_dailink_master: simple-audio-card,cpu {
sound-dai = <&mcasp2>;
system-clock-frequency = <24576000>;//24Mhz:44khz<22579200>;24Mhz:48khz<24576000>;//12Mhz:44khz:<11289600>;
system-clock-id = <MCASP_CLK_HCLK_AUXCLK>;
system-clock-direction = "out";
};
simple-audio-card,codec {
sound-dai = <&sii9022>;
system-clock-frequency = <12000000>;
};
};
We are validating the audio functionality in the kernel of Android 9 by using TinyAlsa.
While exercising audio Playback using Tinyplay for sound card0 (HDMI) we are hitting with the below error and Playback is not happening on the HDMI for Android Pie.
console:/ # tinyplay /sdcard/Music/0267.wav -D 0
Unable to open PCM device 0 (cannot set hw params: Invalid argument)
But for the Audio Codec(TLV320) we are observing that playback is succesfull.
console:/ # tinyplay /sdcard/Music/0267.wav -D 1
Playing sample: 2 ch, 44100 hz, 16 bit
I was wondering if you can help us on identifying the reason behind the error while playing via HDMI?
Please find the attached linux driver for Sil022 HDMI Transmitter driver.
/*
* Copyright (C) 2018 Renesas Electronics
*
* Copyright (C) 2016 Atmel
* Bo Shen <voice.shen@atmel.com>
*
* Authors: Bo Shen <voice.shen@atmel.com>
* Boris Brezillon <boris.brezillon@free-electrons.com>
* Wu, Songjun <Songjun.Wu@atmel.com>
*
*
* Copyright (C) 2010-2011 Freescale Semiconductor, Inc. All Rights Reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License as published by
* the Free Software Foundation; either version 2 of the License, or
* (at your option) any later version.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*/
#include <linux/gpio/consumer.h>
#include <linux/i2c-mux.h>
#include <linux/i2c.h>
#include <linux/module.h>
#include <linux/regmap.h>
#include <linux/clk.h>
#include <drm/drmP.h>
#include <drm/drm_atomic_helper.h>
#include <drm/drm_crtc_helper.h>
#include <drm/drm_edid.h>
#include <sound/hdmi-codec.h>
#include <dt-bindings/sound/sii902x-audio.h>
#define SII902X_TPI_VIDEO_DATA 0x0
#define SII902X_TPI_PIXEL_REPETITION 0x8
#define SII902X_TPI_AVI_PIXEL_REP_BUS_24BIT BIT(5)
#define SII902X_TPI_AVI_PIXEL_REP_RISING_EDGE BIT(4)
#define SII902X_TPI_AVI_PIXEL_REP_4X 3
#define SII902X_TPI_AVI_PIXEL_REP_2X 1
#define SII902X_TPI_AVI_PIXEL_REP_NONE 0
#define SII902X_TPI_CLK_RATIO_HALF (0 << 6)
#define SII902X_TPI_CLK_RATIO_1X (1 << 6)
#define SII902X_TPI_CLK_RATIO_2X (2 << 6)
#define SII902X_TPI_CLK_RATIO_4X (3 << 6)
#define SII902X_TPI_AVI_IN_FORMAT 0x9
#define SII902X_TPI_AVI_INPUT_BITMODE_12BIT BIT(7)
#define SII902X_TPI_AVI_INPUT_DITHER BIT(6)
#define SII902X_TPI_AVI_INPUT_RANGE_LIMITED (2 << 2)
#define SII902X_TPI_AVI_INPUT_RANGE_FULL (1 << 2)
#define SII902X_TPI_AVI_INPUT_RANGE_AUTO (0 << 2)
#define SII902X_TPI_AVI_INPUT_COLORSPACE_BLACK (3 << 0)
#define SII902X_TPI_AVI_INPUT_COLORSPACE_YUV422 (2 << 0)
#define SII902X_TPI_AVI_INPUT_COLORSPACE_YUV444 (1 << 0)
#define SII902X_TPI_AVI_INPUT_COLORSPACE_RGB (0 << 0)
#define SII902X_TPI_AVI_INFOFRAME 0x0c
#define SII902X_SYS_CTRL_DATA 0x1a
#define SII902X_SYS_CTRL_PWR_DWN BIT(4)
#define SII902X_SYS_CTRL_AV_MUTE BIT(3)
#define SII902X_SYS_CTRL_DDC_BUS_REQ BIT(2)
#define SII902X_SYS_CTRL_DDC_BUS_GRTD BIT(1)
#define SII902X_SYS_CTRL_OUTPUT_MODE BIT(0)
#define SII902X_SYS_CTRL_OUTPUT_HDMI 1
#define SII902X_SYS_CTRL_OUTPUT_DVI 0
#define SII902X_REG_CHIPID(n) (0x1b + (n))
#define SII902X_PWR_STATE_CTRL 0x1e
#define SII902X_AVI_POWER_STATE_MSK GENMASK(1, 0)
#define SII902X_AVI_POWER_STATE_D(l) ((l) & SII902X_AVI_POWER_STATE_MSK)
/* Audio */
#define SII902X_TPI_I2S_ENABLE_MAPPING_REG 0x1f
#define SII902X_TPI_I2S_CONFIG_FIFO0 (0 << 0)
#define SII902X_TPI_I2S_CONFIG_FIFO1 (1 << 0)
#define SII902X_TPI_I2S_CONFIG_FIFO2 (2 << 0)
#define SII902X_TPI_I2S_CONFIG_FIFO3 (3 << 0)
#define SII902X_TPI_I2S_LEFT_RIGHT_SWAP (1 << 2)
#define SII902X_TPI_I2S_AUTO_DOWNSAMPLE (1 << 3)
#define SII902X_TPI_I2S_SELECT_SD0 (0 << 4)
#define SII902X_TPI_I2S_SELECT_SD1 (1 << 4)
#define SII902X_TPI_I2S_SELECT_SD2 (2 << 4)
#define SII902X_TPI_I2S_SELECT_SD3 (3 << 4)
#define SII902X_TPI_I2S_FIFO_ENABLE (1 << 7)
#define SII902X_TPI_I2S_INPUT_CONFIG_REG 0x20
#define SII902X_TPI_I2S_FIRST_BIT_SHIFT_YES (0 << 0)
#define SII902X_TPI_I2S_FIRST_BIT_SHIFT_NO (1 << 0)
#define SII902X_TPI_I2S_SD_DIRECTION_MSB_FIRST (0 << 1)
#define SII902X_TPI_I2S_SD_DIRECTION_LSB_FIRST (1 << 1)
#define SII902X_TPI_I2S_SD_JUSTIFY_LEFT (0 << 2)
#define SII902X_TPI_I2S_SD_JUSTIFY_RIGHT (1 << 2)
#define SII902X_TPI_I2S_WS_POLARITY_LOW (0 << 3)
#define SII902X_TPI_I2S_WS_POLARITY_HIGH (1 << 3)
#define SII902X_TPI_I2S_MCLK_MULTIPLIER_128 (0 << 4)
#define SII902X_TPI_I2S_MCLK_MULTIPLIER_256 (1 << 4)
#define SII902X_TPI_I2S_MCLK_MULTIPLIER_384 (2 << 4)
#define SII902X_TPI_I2S_MCLK_MULTIPLIER_512 (3 << 4)
#define SII902X_TPI_I2S_MCLK_MULTIPLIER_768 (4 << 4)
#define SII902X_TPI_I2S_MCLK_MULTIPLIER_1024 (5 << 4)
#define SII902X_TPI_I2S_MCLK_MULTIPLIER_1152 (6 << 4)
#define SII902X_TPI_I2S_MCLK_MULTIPLIER_192 (7 << 4)
#define SII902X_TPI_I2S_SCK_EDGE_FALLING (0 << 7)
#define SII902X_TPI_I2S_SCK_EDGE_RISING (1 << 7)
#define SII902X_TPI_I2S_STRM_HDR_BASE 0x21
#define SII902X_TPI_I2S_STRM_HDR_SIZE 5
#define SII902X_TPI_AUDIO_CONFIG_BYTE2_REG 0x26
#define SII902X_TPI_AUDIO_CODING_STREAM_HEADER (0 << 0)
#define SII902X_TPI_AUDIO_CODING_PCM (1 << 0)
#define SII902X_TPI_AUDIO_CODING_AC3 (2 << 0)
#define SII902X_TPI_AUDIO_CODING_MPEG1 (3 << 0)
#define SII902X_TPI_AUDIO_CODING_MP3 (4 << 0)
#define SII902X_TPI_AUDIO_CODING_MPEG2 (5 << 0)
#define SII902X_TPI_AUDIO_CODING_AAC (6 << 0)
#define SII902X_TPI_AUDIO_CODING_DTS (7 << 0)
#define SII902X_TPI_AUDIO_CODING_ATRAC (8 << 0)
#define SII902X_TPI_AUDIO_MUTE_DISABLE (0 << 4)
#define SII902X_TPI_AUDIO_MUTE_ENABLE (1 << 4)
#define SII902X_TPI_AUDIO_LAYOUT_2_CHANNELS (0 << 5)
#define SII902X_TPI_AUDIO_LAYOUT_8_CHANNELS (1 << 5)
#define SII902X_TPI_AUDIO_INTERFACE_DISABLE (0 << 6)
#define SII902X_TPI_AUDIO_INTERFACE_SPDIF (1 << 6)
#define SII902X_TPI_AUDIO_INTERFACE_I2S (2 << 6)
#define SII902X_TPI_AUDIO_CONFIG_BYTE3_REG 0x27
#define SII902X_TPI_AUDIO_CHANNEL_STREAM (0 << 0)
#define SII902X_TPI_AUDIO_2_CHANNEL (1 << 0)
#define SII902X_TPI_AUDIO_8_CHANNEL (7 << 0)
#define SII902X_TPI_AUDIO_FREQ_STREAM (0 << 3)
#define SII902X_TPI_AUDIO_FREQ_32KHZ (1 << 3)
#define SII902X_TPI_AUDIO_FREQ_44KHZ (2 << 3)
#define SII902X_TPI_AUDIO_FREQ_48KHZ (3 << 3)
#define SII902X_TPI_AUDIO_FREQ_88KHZ (4 << 3)
#define SII902X_TPI_AUDIO_FREQ_96KHZ (5 << 3)
#define SII902X_TPI_AUDIO_FREQ_176KHZ (6 << 3)
#define SII902X_TPI_AUDIO_FREQ_192KHZ (7 << 3)
#define SII902X_TPI_AUDIO_SAMPLE_SIZE_STREAM (0 << 6)
#define SII902X_TPI_AUDIO_SAMPLE_SIZE_16 (1 << 6)
#define SII902X_TPI_AUDIO_SAMPLE_SIZE_20 (2 << 6)
#define SII902X_TPI_AUDIO_SAMPLE_SIZE_24 (3 << 6)
#define SII902X_TPI_AUDIO_CONFIG_BYTE4_REG 0x28
#define SII902X_INT_ENABLE 0x3c
#define SII902X_INT_STATUS 0x3d
#define SII902X_HOTPLUG_EVENT BIT(0)
#define SII902X_PLUGGED_STATUS BIT(2)
#define SII902X_REG_TPI_RQB 0xc7
/* Indirect internal register access */
#define SII902X_IND_SET_PAGE 0xbc
#define SII902X_IND_OFFSET 0xbd
#define SII902X_IND_VALUE 0xbe
#define SII902X_TPI_MISC_INFOFRAME_BASE 0xbf
#define SII902X_TPI_MISC_INFOFRAME_END 0xde
#define SII902X_TPI_MISC_INFOFRAME_SIZE \
(SII902X_TPI_MISC_INFOFRAME_END - SII902X_TPI_MISC_INFOFRAME_BASE)
#define SII902X_I2C_BUS_ACQUISITION_TIMEOUT_MS 500
struct sii902x {
struct i2c_client *i2c;
struct regmap *regmap;
struct drm_bridge bridge;
struct drm_connector connector;
struct gpio_desc *reset_gpio;
struct i2c_mux_core *i2cmux;
struct mutex mutex;
struct sii902x_audio {
struct platform_device *pdev;
u8 channels;
struct clk *mclk;
bool mclk_enabled;
u32 i2s_fifo_routing[4];
} audio;
};
static int sii902x_read_unlocked(struct i2c_client *i2c, u8 reg, u8 *val)
{
union i2c_smbus_data data;
int ret;
ret = __i2c_smbus_xfer(i2c->adapter, i2c->addr, i2c->flags,
I2C_SMBUS_READ, reg, I2C_SMBUS_BYTE_DATA, &data);
if (ret < 0)
return ret;
*val = data.byte;
return 0;
}
static int sii902x_write_unlocked(struct i2c_client *i2c, u8 reg, u8 val)
{
union i2c_smbus_data data;
data.byte = val;
return __i2c_smbus_xfer(i2c->adapter, i2c->addr, i2c->flags,
I2C_SMBUS_WRITE, reg, I2C_SMBUS_BYTE_DATA,
&data);
}
static int sii902x_update_bits_unlocked(struct i2c_client *i2c, u8 reg, u8 mask,
u8 val)
{
int ret;
u8 status;
ret = sii902x_read_unlocked(i2c, reg, &status);
if (ret)
return ret;
status &= ~mask;
status |= val & mask;
return sii902x_write_unlocked(i2c, reg, status);
}
static inline struct sii902x *bridge_to_sii902x(struct drm_bridge *bridge)
{
return container_of(bridge, struct sii902x, bridge);
}
static inline struct sii902x *connector_to_sii902x(struct drm_connector *con)
{
return container_of(con, struct sii902x, connector);
}
static void sii902x_reset(struct sii902x *sii902x)
{
if (!sii902x->reset_gpio)
return;
gpiod_set_value(sii902x->reset_gpio, 1);
/* The datasheet says treset-min = 100us. Make it 150us to be sure. */
usleep_range(150, 200);
gpiod_set_value(sii902x->reset_gpio, 0);
}
static enum drm_connector_status
sii902x_connector_detect(struct drm_connector *connector, bool force)
{
struct sii902x *sii902x = connector_to_sii902x(connector);
unsigned int status;
mutex_lock(&sii902x->mutex);
regmap_read(sii902x->regmap, SII902X_INT_STATUS, &status);
mutex_unlock(&sii902x->mutex);
return (status & SII902X_PLUGGED_STATUS) ?
connector_status_connected : connector_status_disconnected;
}
static const struct drm_connector_funcs sii902x_connector_funcs = {
.detect = sii902x_connector_detect,
.fill_modes = drm_helper_probe_single_connector_modes,
.destroy = drm_connector_cleanup,
.reset = drm_atomic_helper_connector_reset,
.atomic_duplicate_state = drm_atomic_helper_connector_duplicate_state,
.atomic_destroy_state = drm_atomic_helper_connector_destroy_state,
};
static int sii902x_get_modes(struct drm_connector *connector)
{
struct sii902x *sii902x = connector_to_sii902x(connector);
u32 bus_format = MEDIA_BUS_FMT_RGB888_1X24;
struct edid *edid;
u8 output_mode = SII902X_SYS_CTRL_OUTPUT_DVI;
int num = 0, ret;
mutex_lock(&sii902x->mutex);
edid = drm_get_edid(connector, sii902x->i2cmux->adapter[0]);
drm_connector_update_edid_property(connector, edid);
if (edid) {
if (drm_detect_hdmi_monitor(edid))
output_mode = SII902X_SYS_CTRL_OUTPUT_HDMI;
num = drm_add_edid_modes(connector, edid);
kfree(edid);
}
ret = drm_display_info_set_bus_formats(&connector->display_info,
&bus_format, 1);
if (ret)
goto error_out;
ret = regmap_update_bits(sii902x->regmap, SII902X_SYS_CTRL_DATA,
SII902X_SYS_CTRL_OUTPUT_MODE, output_mode);
if (ret)
goto error_out;
ret = num;
error_out:
mutex_unlock(&sii902x->mutex);
return ret;
}
static enum drm_mode_status sii902x_mode_valid(struct drm_connector *connector,
struct drm_display_mode *mode)
{
/* TODO: check mode */
return MODE_OK;
}
static const struct drm_connector_helper_funcs sii902x_connector_helper_funcs = {
.get_modes = sii902x_get_modes,
.mode_valid = sii902x_mode_valid,
};
static void sii902x_bridge_disable(struct drm_bridge *bridge)
{
struct sii902x *sii902x = bridge_to_sii902x(bridge);
mutex_lock(&sii902x->mutex);
regmap_update_bits(sii902x->regmap, SII902X_SYS_CTRL_DATA,
SII902X_SYS_CTRL_PWR_DWN,
SII902X_SYS_CTRL_PWR_DWN);
mutex_unlock(&sii902x->mutex);
}
static void sii902x_bridge_enable(struct drm_bridge *bridge)
{
struct sii902x *sii902x = bridge_to_sii902x(bridge);
mutex_lock(&sii902x->mutex);
regmap_update_bits(sii902x->regmap, SII902X_PWR_STATE_CTRL,
SII902X_AVI_POWER_STATE_MSK,
SII902X_AVI_POWER_STATE_D(0));
regmap_update_bits(sii902x->regmap, SII902X_SYS_CTRL_DATA,
SII902X_SYS_CTRL_PWR_DWN, 0);
mutex_unlock(&sii902x->mutex);
}
static void sii902x_bridge_mode_set(struct drm_bridge *bridge,
struct drm_display_mode *mode,
struct drm_display_mode *adj)
{
struct sii902x *sii902x = bridge_to_sii902x(bridge);
struct regmap *regmap = sii902x->regmap;
u8 buf[HDMI_INFOFRAME_SIZE(AVI)];
struct hdmi_avi_infoframe frame;
u16 pixel_clock_10kHz = adj->clock / 10;
int ret;
buf[0] = pixel_clock_10kHz & 0xff;
buf[1] = pixel_clock_10kHz >> 8;
buf[2] = adj->vrefresh;
buf[3] = 0x00;
buf[4] = adj->hdisplay;
buf[5] = adj->hdisplay >> 8;
buf[6] = adj->vdisplay;
buf[7] = adj->vdisplay >> 8;
buf[8] = SII902X_TPI_CLK_RATIO_1X | SII902X_TPI_AVI_PIXEL_REP_NONE |
SII902X_TPI_AVI_PIXEL_REP_BUS_24BIT;
buf[9] = SII902X_TPI_AVI_INPUT_RANGE_AUTO |
SII902X_TPI_AVI_INPUT_COLORSPACE_RGB;
mutex_lock(&sii902x->mutex);
ret = regmap_bulk_write(regmap, SII902X_TPI_VIDEO_DATA, buf, 10);
if (ret)
goto out;
ret = drm_hdmi_avi_infoframe_from_display_mode(&frame, adj, false);
if (ret < 0) {
DRM_ERROR("couldn't fill AVI infoframe\n");
goto out;
}
ret = hdmi_avi_infoframe_pack(&frame, buf, sizeof(buf));
if (ret < 0) {
DRM_ERROR("failed to pack AVI infoframe: %d\n", ret);
goto out;
}
/* Do not send the infoframe header, but keep the CRC field. */
regmap_bulk_write(regmap, SII902X_TPI_AVI_INFOFRAME,
buf + HDMI_INFOFRAME_HEADER_SIZE - 1,
HDMI_AVI_INFOFRAME_SIZE + 1);
out:
mutex_unlock(&sii902x->mutex);
}
static int sii902x_bridge_attach(struct drm_bridge *bridge)
{
struct sii902x *sii902x = bridge_to_sii902x(bridge);
struct drm_device *drm = bridge->dev;
int ret;
drm_connector_helper_add(&sii902x->connector,
&sii902x_connector_helper_funcs);
if (!drm_core_check_feature(drm, DRIVER_ATOMIC)) {
dev_err(&sii902x->i2c->dev,
"sii902x driver is only compatible with DRM devices supporting atomic updates\n");
return -ENOTSUPP;
}
ret = drm_connector_init(drm, &sii902x->connector,
&sii902x_connector_funcs,
DRM_MODE_CONNECTOR_HDMIA);
if (ret)
return ret;
if (sii902x->i2c->irq > 0)
sii902x->connector.polled = DRM_CONNECTOR_POLL_HPD;
else
sii902x->connector.polled = DRM_CONNECTOR_POLL_CONNECT;
drm_connector_attach_encoder(&sii902x->connector, bridge->encoder);
return 0;
}
static const struct drm_bridge_funcs sii902x_bridge_funcs = {
.attach = sii902x_bridge_attach,
.mode_set = sii902x_bridge_mode_set,
.disable = sii902x_bridge_disable,
.enable = sii902x_bridge_enable,
};
static int sii902x_mute(struct sii902x *sii902x, int mute)
{
u8 channel_layout = sii902x->audio.channels > 2 ?
SII902X_TPI_AUDIO_LAYOUT_8_CHANNELS :
SII902X_TPI_AUDIO_LAYOUT_2_CHANNELS;
struct device *dev = &sii902x->i2c->dev;
int ret;
if (mute) {
dev_dbg(dev, "%s: Muted (%d)\n", __func__, mute);
ret = regmap_write(sii902x->regmap,
SII902X_TPI_AUDIO_CONFIG_BYTE2_REG,
SII902X_TPI_AUDIO_INTERFACE_I2S |
channel_layout |
SII902X_TPI_AUDIO_MUTE_ENABLE |
SII902X_TPI_AUDIO_CODING_PCM);
} else {
dev_dbg(dev, "%s: Unmuted (%d)\n", __func__, mute);
ret = regmap_write(sii902x->regmap,
SII902X_TPI_AUDIO_CONFIG_BYTE2_REG,
SII902X_TPI_AUDIO_INTERFACE_I2S |
channel_layout |
SII902X_TPI_AUDIO_MUTE_DISABLE |
SII902X_TPI_AUDIO_CODING_PCM);
}
return ret;
}
static const unsigned int sii902x_mclk_div_table[] = {
128, 256, 384, 512, 768, 1024, 1152, 192 };
static int sii902x_select_mclk_div(u8 *i2s_config_reg, unsigned int rate,
unsigned int mclk)
{
int distance = 100000;
u8 i, nearest = 0;
for (i = 0; i < ARRAY_SIZE(sii902x_mclk_div_table); i++) {
unsigned int div = mclk / rate;
if (abs(div - sii902x_mclk_div_table[i]) < distance) {
nearest = i;
distance = abs(div - sii902x_mclk_div_table[i]);
}
if (div == sii902x_mclk_div_table[i])
break;
}
*i2s_config_reg |= nearest << 4;
if (i == ARRAY_SIZE(sii902x_mclk_div_table))
return sii902x_mclk_div_table[nearest];
return 0;
}
static int sii902x_audio_hw_params(struct device *dev, void *data,
struct hdmi_codec_daifmt *daifmt,
struct hdmi_codec_params *params)
{
struct sii902x *sii902x = dev_get_drvdata(dev);
u8 i2s_config_reg = SII902X_TPI_I2S_SD_DIRECTION_MSB_FIRST;
u8 config_byte3_reg = SII902X_TPI_AUDIO_CHANNEL_STREAM;
u8 infoframe_buf[HDMI_INFOFRAME_SIZE(AUDIO)];
unsigned long mclk_rate;
int i, ret;
if (daifmt->bit_clk_master || daifmt->frame_clk_master) {
dev_dbg(dev, "%s: I2S master mode not supported\n", __func__);
return -EINVAL;
}
switch (daifmt->fmt) {
case HDMI_I2S:
i2s_config_reg |= SII902X_TPI_I2S_FIRST_BIT_SHIFT_YES |
SII902X_TPI_I2S_SD_JUSTIFY_LEFT;
break;
case HDMI_RIGHT_J:
i2s_config_reg |= SII902X_TPI_I2S_SD_JUSTIFY_RIGHT;
break;
case HDMI_LEFT_J:
i2s_config_reg |= SII902X_TPI_I2S_SD_JUSTIFY_LEFT;
break;
default:
dev_dbg(dev, "%s: Unsupported i2s format %u\n", __func__,
daifmt->fmt);
return -EINVAL;
}
if (daifmt->bit_clk_inv)
i2s_config_reg |= SII902X_TPI_I2S_SCK_EDGE_FALLING;
else
i2s_config_reg |= SII902X_TPI_I2S_SCK_EDGE_RISING;
if (daifmt->frame_clk_inv)
i2s_config_reg |= SII902X_TPI_I2S_WS_POLARITY_LOW;
else
i2s_config_reg |= SII902X_TPI_I2S_WS_POLARITY_HIGH;
switch (params->sample_width) {
case 16:
config_byte3_reg |= SII902X_TPI_AUDIO_SAMPLE_SIZE_16;
break;
case 20:
config_byte3_reg |= SII902X_TPI_AUDIO_SAMPLE_SIZE_20;
break;
case 24:
case 32:
config_byte3_reg |= SII902X_TPI_AUDIO_SAMPLE_SIZE_24;
break;
default:
dev_err(dev, "%s: Unsupported sample width %u\n", __func__,
params->sample_width);
return -EINVAL;
};
ret = clk_prepare_enable(sii902x->audio.mclk);
if (ret) {
dev_err(dev, "Enabling mclk failed: %d\n", ret);
return ret;
}
sii902x->audio.mclk_enabled = true;
mclk_rate = clk_get_rate(sii902x->audio.mclk);
ret = sii902x_select_mclk_div(&i2s_config_reg, params->sample_rate,
mclk_rate);
if (ret)
dev_dbg(dev, "Inaccurate reference clock (%ld/%d != %u)\n",
mclk_rate, ret, params->sample_rate);
sii902x->audio.channels = params->channels;
mutex_lock(&sii902x->mutex);
ret = sii902x_mute(sii902x, true);
if (ret < 0)
goto out;
ret = regmap_write(sii902x->regmap, SII902X_TPI_I2S_INPUT_CONFIG_REG,
i2s_config_reg);
if (ret)
goto out;
for (i = 0; i < ARRAY_SIZE(sii902x->audio.i2s_fifo_routing); i++)
regmap_write(sii902x->regmap,
SII902X_TPI_I2S_ENABLE_MAPPING_REG,
sii902x->audio.i2s_fifo_routing[i]);
ret = regmap_write(sii902x->regmap, SII902X_TPI_AUDIO_CONFIG_BYTE3_REG,
config_byte3_reg);
if (ret)
goto out;
ret = regmap_bulk_write(sii902x->regmap, SII902X_TPI_I2S_STRM_HDR_BASE,
params->iec.status,
min((size_t) SII902X_TPI_I2S_STRM_HDR_SIZE,
sizeof(params->iec.status)));
if (ret)
goto out;
ret = hdmi_audio_infoframe_pack(¶ms->cea, infoframe_buf,
sizeof(infoframe_buf));
if (ret < 0) {
dev_err(dev, "%s: Failed to pack audio infoframe: %d\n",
__func__, ret);
goto out;
}
ret = regmap_bulk_write(sii902x->regmap,
SII902X_TPI_MISC_INFOFRAME_BASE,
infoframe_buf,
min(ret, SII902X_TPI_MISC_INFOFRAME_SIZE));
if (ret)
goto out;
/* Decode Level 0 Packets */
ret = regmap_write(sii902x->regmap, SII902X_IND_SET_PAGE, 0x02);
if (ret)
goto out;
ret = regmap_write(sii902x->regmap, SII902X_IND_OFFSET, 0x24);
if (ret)
goto out;
ret = regmap_write(sii902x->regmap, SII902X_IND_VALUE, 0x02);
if (ret)
goto out;
dev_dbg(dev, "%s: hdmi audio enabled\n", __func__);
out:
mutex_unlock(&sii902x->mutex);
if (ret) {
clk_disable_unprepare(sii902x->audio.mclk);
dev_err(dev, "%s: hdmi audio enable failed: %d\n", __func__,
ret);
}
return ret;
}
static void sii902x_audio_shutdown(struct device *dev, void *data)
{
struct sii902x *sii902x = dev_get_drvdata(dev);
mutex_lock(&sii902x->mutex);
regmap_write(sii902x->regmap, SII902X_TPI_AUDIO_CONFIG_BYTE2_REG,
SII902X_TPI_AUDIO_INTERFACE_DISABLE);
mutex_unlock(&sii902x->mutex);
if (sii902x->audio.mclk_enabled) {
clk_disable_unprepare(sii902x->audio.mclk);
sii902x->audio.mclk_enabled = false;
}
}
int sii902x_audio_digital_mute(struct device *dev, void *data, bool enable)
{
struct sii902x *sii902x = dev_get_drvdata(dev);
mutex_lock(&sii902x->mutex);
sii902x_mute(sii902x, enable);
mutex_unlock(&sii902x->mutex);
return 0;
}
static int sii902x_audio_get_eld(struct device *dev, void *data,
uint8_t *buf, size_t len)
{
struct sii902x *sii902x = dev_get_drvdata(dev);
mutex_lock(&sii902x->mutex);
memcpy(buf, sii902x->connector.eld,
min(sizeof(sii902x->connector.eld), len));
mutex_unlock(&sii902x->mutex);
return 0;
}
static const struct hdmi_codec_ops sii902x_audio_codec_ops = {
.hw_params = sii902x_audio_hw_params,
.audio_shutdown = sii902x_audio_shutdown,
.digital_mute = sii902x_audio_digital_mute,
.get_eld = sii902x_audio_get_eld,
};
static int sii902x_audio_codec_init(struct sii902x *sii902x,
struct device *dev)
{
static const u8 i2s_fifo_defaults[] = {
SII902X_TPI_I2S_CONFIG_FIFO0,
SII902X_TPI_I2S_CONFIG_FIFO1,
SII902X_TPI_I2S_CONFIG_FIFO2,
SII902X_TPI_I2S_CONFIG_FIFO3,
};
struct hdmi_codec_pdata codec_data = {
.ops = &sii902x_audio_codec_ops,
.i2s = 1, /* Only i2s support for now. */
.spdif = 0,
.max_i2s_channels = 0,
};
int ret, i;
ret = of_property_read_u32_array(dev->of_node, "i2s-fifo-routing",
sii902x->audio.i2s_fifo_routing,
ARRAY_SIZE(sii902x->audio.i2s_fifo_routing));
if (ret != 0) {
if (ret == -EINVAL)
dev_dbg(dev, "%s: No \"i2s-fifo-routing\", no audio\n",
__func__);
else
dev_err(dev,
"%s: Error gettin \"i2s-fifo-routing\": %d\n",
__func__, ret);
return 0;
}
/* sii902x->audio.mclk = devm_clk_get(dev, NULL);
if (IS_ERR(sii902x->audio.mclk)) {
dev_err(dev, "%s: No clock (audio mclk) found: %ld\n",
__func__, PTR_ERR(sii902x->audio.mclk));
return 0;
} */
for (i = 0; i < ARRAY_SIZE(sii902x->audio.i2s_fifo_routing); i++) {
if (sii902x->audio.i2s_fifo_routing[i] & ENABLE_BIT)
codec_data.max_i2s_channels += 2;
sii902x->audio.i2s_fifo_routing[i] |= i2s_fifo_defaults[i];
}
sii902x->audio.pdev = platform_device_register_data(
dev, HDMI_CODEC_DRV_NAME, PLATFORM_DEVID_AUTO,
&codec_data, sizeof(codec_data));
return PTR_ERR_OR_ZERO(sii902x->audio.pdev);
}
static const struct regmap_range sii902x_volatile_ranges[] = {
{ .range_min = 0, .range_max = 0xff },
};
static const struct regmap_access_table sii902x_volatile_table = {
.yes_ranges = sii902x_volatile_ranges,
.n_yes_ranges = ARRAY_SIZE(sii902x_volatile_ranges),
};
static const struct regmap_config sii902x_regmap_config = {
.reg_bits = 8,
.val_bits = 8,
.max_register = SII902X_TPI_MISC_INFOFRAME_END,
.volatile_table = &sii902x_volatile_table,
.cache_type = REGCACHE_NONE,
};
static irqreturn_t sii902x_interrupt(int irq, void *data)
{
struct sii902x *sii902x = data;
unsigned int status = 0;
regmap_read(sii902x->regmap, SII902X_INT_STATUS, &status);
regmap_write(sii902x->regmap, SII902X_INT_STATUS, status);
if ((status & SII902X_HOTPLUG_EVENT) && sii902x->bridge.dev)
drm_helper_hpd_irq_event(sii902x->bridge.dev);
return IRQ_HANDLED;
}
/*
* The purpose of sii902x_i2c_bypass_select is to enable the pass through
* mode of the HDMI transmitter. Do not use regmap from within this function,
* only use sii902x_*_unlocked functions to read/modify/write registers.
* We are holding the parent adapter lock here, keep this in mind before
* adding more i2c transactions.
*
* Also, since SII902X_SYS_CTRL_DATA is used with regmap_update_bits elsewhere
* in this driver, we need to make sure that we only touch 0x1A[2:1] from
* within sii902x_i2c_bypass_select and sii902x_i2c_bypass_deselect, and that
* we leave the remaining bits as we have found them.
*/
static int sii902x_i2c_bypass_select(struct i2c_mux_core *mux, u32 chan_id)
{
struct sii902x *sii902x = i2c_mux_priv(mux);
struct device *dev = &sii902x->i2c->dev;
unsigned long timeout;
u8 status;
int ret;
ret = sii902x_update_bits_unlocked(sii902x->i2c, SII902X_SYS_CTRL_DATA,
SII902X_SYS_CTRL_DDC_BUS_REQ,
SII902X_SYS_CTRL_DDC_BUS_REQ);
if (ret)
return ret;
timeout = jiffies +
msecs_to_jiffies(SII902X_I2C_BUS_ACQUISITION_TIMEOUT_MS);
do {
ret = sii902x_read_unlocked(sii902x->i2c, SII902X_SYS_CTRL_DATA,
&status);
if (ret)
return ret;
} while (!(status & SII902X_SYS_CTRL_DDC_BUS_GRTD) &&
time_before(jiffies, timeout));
if (!(status & SII902X_SYS_CTRL_DDC_BUS_GRTD)) {
dev_err(dev, "Failed to acquire the i2c bus\n");
return -ETIMEDOUT;
}
return sii902x_write_unlocked(sii902x->i2c, SII902X_SYS_CTRL_DATA,
status);
}
/*
* The purpose of sii902x_i2c_bypass_deselect is to disable the pass through
* mode of the HDMI transmitter. Do not use regmap from within this function,
* only use sii902x_*_unlocked functions to read/modify/write registers.
* We are holding the parent adapter lock here, keep this in mind before
* adding more i2c transactions.
*
* Also, since SII902X_SYS_CTRL_DATA is used with regmap_update_bits elsewhere
* in this driver, we need to make sure that we only touch 0x1A[2:1] from
* within sii902x_i2c_bypass_select and sii902x_i2c_bypass_deselect, and that
* we leave the remaining bits as we have found them.
*/
static int sii902x_i2c_bypass_deselect(struct i2c_mux_core *mux, u32 chan_id)
{
struct sii902x *sii902x = i2c_mux_priv(mux);
struct device *dev = &sii902x->i2c->dev;
unsigned long timeout;
unsigned int retries;
u8 status;
int ret;
/*
* When the HDMI transmitter is in pass through mode, we need an
* (undocumented) additional delay between STOP and START conditions
* to guarantee the bus won't get stuck.
*/
udelay(30);
/*
* Sometimes the I2C bus can stall after failure to use the
* EDID channel. Retry a few times to see if things clear
* up, else continue anyway.
*/
retries = 5;
do {
ret = sii902x_read_unlocked(sii902x->i2c, SII902X_SYS_CTRL_DATA,
&status);
retries--;
} while (ret && retries);
if (ret) {
dev_err(dev, "failed to read status (%d)\n", ret);
return ret;
}
ret = sii902x_update_bits_unlocked(sii902x->i2c, SII902X_SYS_CTRL_DATA,
SII902X_SYS_CTRL_DDC_BUS_REQ |
SII902X_SYS_CTRL_DDC_BUS_GRTD, 0);
if (ret)
return ret;
timeout = jiffies +
msecs_to_jiffies(SII902X_I2C_BUS_ACQUISITION_TIMEOUT_MS);
do {
ret = sii902x_read_unlocked(sii902x->i2c, SII902X_SYS_CTRL_DATA,
&status);
if (ret)
return ret;
} while (status & (SII902X_SYS_CTRL_DDC_BUS_REQ |
SII902X_SYS_CTRL_DDC_BUS_GRTD) &&
time_before(jiffies, timeout));
if (status & (SII902X_SYS_CTRL_DDC_BUS_REQ |
SII902X_SYS_CTRL_DDC_BUS_GRTD)) {
dev_err(dev, "failed to release the i2c bus\n");
return -ETIMEDOUT;
}
return 0;
}
static const struct drm_bridge_timings default_sii902x_timings = {
.input_bus_flags = DRM_BUS_FLAG_PIXDATA_SAMPLE_NEGEDGE
| DRM_BUS_FLAG_SYNC_SAMPLE_NEGEDGE
| DRM_BUS_FLAG_DE_HIGH,
};
static int sii902x_probe(struct i2c_client *client,
const struct i2c_device_id *id)
{
struct device *dev = &client->dev;
unsigned int status = 0;
struct sii902x *sii902x;
u8 chipid[4];
int ret;
ret = i2c_check_functionality(client->adapter,
I2C_FUNC_SMBUS_BYTE_DATA);
if (!ret) {
dev_err(dev, "I2C adapter not suitable\n");
return -EIO;
}
sii902x = devm_kzalloc(dev, sizeof(*sii902x), GFP_KERNEL);
if (!sii902x)
return -ENOMEM;
sii902x->i2c = client;
sii902x->regmap = devm_regmap_init_i2c(client, &sii902x_regmap_config);
if (IS_ERR(sii902x->regmap))
return PTR_ERR(sii902x->regmap);
sii902x->reset_gpio = devm_gpiod_get_optional(dev, "reset",
GPIOD_OUT_LOW);
if (IS_ERR(sii902x->reset_gpio)) {
dev_err(dev, "Failed to retrieve/request reset gpio: %ld\n",
PTR_ERR(sii902x->reset_gpio));
return PTR_ERR(sii902x->reset_gpio);
}
/* protect audio and video functions from each other */
mutex_init(&sii902x->mutex);
sii902x_reset(sii902x);
ret = regmap_write(sii902x->regmap, SII902X_REG_TPI_RQB, 0x0);
if (ret)
return ret;
ret = regmap_bulk_read(sii902x->regmap, SII902X_REG_CHIPID(0),
&chipid, 4);
if (ret) {
dev_err(dev, "regmap_read failed %d\n", ret);
return ret;
}
if (chipid[0] != 0xb0) {
dev_err(dev, "Invalid chipid: %02x (expecting 0xb0)\n",
chipid[0]);
return -EINVAL;
}
/* Clear all pending interrupts */
regmap_read(sii902x->regmap, SII902X_INT_STATUS, &status);
regmap_write(sii902x->regmap, SII902X_INT_STATUS, status);
if (client->irq > 0) {
regmap_write(sii902x->regmap, SII902X_INT_ENABLE,
SII902X_HOTPLUG_EVENT);
ret = devm_request_threaded_irq(dev, client->irq, NULL,
sii902x_interrupt,
IRQF_ONESHOT, dev_name(dev),
sii902x);
if (ret)
return ret;
}
sii902x->bridge.funcs = &sii902x_bridge_funcs;
sii902x->bridge.of_node = dev->of_node;
sii902x->bridge.timings = &default_sii902x_timings;
drm_bridge_add(&sii902x->bridge);
sii902x_audio_codec_init(sii902x, dev);
i2c_set_clientdata(client, sii902x);
sii902x->i2cmux = i2c_mux_alloc(client->adapter, dev,
1, 0, I2C_MUX_GATE,
sii902x_i2c_bypass_select,
sii902x_i2c_bypass_deselect);
if (!sii902x->i2cmux)
return -ENOMEM;
sii902x->i2cmux->priv = sii902x;
return i2c_mux_add_adapter(sii902x->i2cmux, 0, 0, 0);
}
static int sii902x_remove(struct i2c_client *client)
{
struct sii902x *sii902x = i2c_get_clientdata(client);
i2c_mux_del_adapters(sii902x->i2cmux);
drm_bridge_remove(&sii902x->bridge);
return 0;
}
static const struct of_device_id sii902x_dt_ids[] = {
{ .compatible = "sil,sii9022", },
{ }
};
MODULE_DEVICE_TABLE(of, sii902x_dt_ids);
static const struct i2c_device_id sii902x_i2c_ids[] = {
{ "sii9022", 0 },
{ },
};
MODULE_DEVICE_TABLE(i2c, sii902x_i2c_ids);
static struct i2c_driver sii902x_driver = {
.probe = sii902x_probe,
.remove = sii902x_remove,
.driver = {
.name = "sii902x",
.of_match_table = sii902x_dt_ids,
},
.id_table = sii902x_i2c_ids,
};
module_i2c_driver(sii902x_driver);
MODULE_AUTHOR("Boris Brezillon <boris.brezillon@free-electrons.com>");
MODULE_DESCRIPTION("SII902x RGB -> HDMI bridges");
MODULE_LICENSE("GPL");
Note: For Arago Distribution we are not seeing any error while using gst-play-1.0 for HDMI and were able to get the audio playback successful. seems the issue is with Tinyalsa and tinyalsa library is using by the audio HAL of the Android we need the fix this issue to make the android working for the Audio on HDMI
Regards,
Ramakrishna Nimmala