Part Number: BEAGLEBOARD-X15
HI.
We tried repo syncing(./repo sync) to download the SDK(/ti-processor-sdk-android-am57xx-evm-06.01.00.08/board-support/aosp-9.0)
from the company office
| fatal: unable to connect to git.ti.com: git.ti.com[0: 198.47.28.208]: errno=Connection refused |
The message above is displayed.
The code was received but I'm not sure if it was received normally.
Checking if it is an internal firewall.
If it's a firewall, which port or IP should I disable?
Beat Regards
CHOI