Part Number: AM3352
Hi champs:
Please read this.
https://e2e.ti.com/support/processors/f/791/t/297550?AM335X-eMMC-boot-problem-with-SD-card-inserted
We have a customer MPed AM335, and they want to fix the boot sequence no matter if the SD card is inserted or not.
In short, the current situation is:
When the SD card is inserted before booting, and press power on,
SD card will be in this file: /dev/mmcblk0
eMMc will be in this file: /dev/mmcblk1
When the SD card is "inserted" before booting, and press power on,
Then, eMMc will be in this file: /dev/mmcblk0
Then they insert the SD card,
The eMMc will be in this file: /dev/mmcblk1
The customer needs the SD card / EMMC will stay the fixed mmcblock forever, how to modify the code in the current version SDK if we refer to the E2E link as the above?
THanks.
BR Rio