This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding EDMA channel and slot allocation

Hi,

 

I looked at the file devices-da8xxx.c, there is a structure where we  do rsv_channel & rsv_slot,  if i need to reserve channels 0 to 5 , 18, 19  and slots 0 to 5, 18,19, 35 ,36 , then how do i specify them in the stucture

  • Hi,

    Comments in the code suggest that the first member is the offset and the second member is the number of channels/slots to be reserved. So in your case if you are willing to reserve channel 0 to 5 you should provide the first member as 0 and second member as 6.

    Regards, Sudhakar