Part Number: AM5728
Daisuke Maeda said:
Our customer has not solved the issue discussed in the previous thread. The issue that SATA controller not detects an attached drive occurs on boards of about 250, but the rate of incidence on each board is very low. Our customer is concerned that some of the errata (i783, i807, i808, i809) for SATA may be left in the SATA driver, but wants to apply minimal modifications to the software because the board is in mass production.
The issue does not occur on many in 10K units.
Can the incidence rate of each errata (i783, i807, i808, i809) vary by device or lot?
Our customer will not modify the software until they understand that the issue may be due to errata.
Best regards,
Daisuke