Hi HS I/F forum,
I had a question about the HDMI output capabilities for OMAP4. How flexible is the frame buffer for the HDMI output? For example, can we use the RGB output to drive a 1280x800 display and HDMI out to drive an independent image, something like another 1280x800 display or 800x600? My initial thought is that we should be able to use an independent frame buffer for each display, since we won’t be using the DSI outputs.
Also, is TI aware of an IC which can translate HDMI to LVDS (TIA/EIA-644)?
This is a question that originated from our customer: Garmin.