I need help in generating an interrupt on DM6437 pin GPIO4 - GP[4]
I set my TConf as
bios.HWI.instance("HWI_INT13").interruptSelectNumber = 68;
bios.HWI.instance("HWI_INT13").fxn = prog.extern("SWC_carrier_freq");
bios.HWI.instance("HWI_INT13").useDispatcher = 1;
I also configured the register GPIO BINTEN
but still my IRQ is not triggered
Here is the code for my register configuration
CSL_SysctlRegsOvly sysRegs = (CSL_SysctlRegsOvly)CSL_SYS_0_REGS;
CSL_FINST(sysRegs-> PINMUX1, SYS_PINMUX1_PWM1BK, RESETVAL);
but still my SwC_Carrier_freq function is not being triggered
CSL_GpioRegsOvly gpioRegs = (CSL_GpioRegsOvly)CSL_GPIO_0_REGS;
CSL_FINST(gpioRegs-> BINTEN, GPIO_BINTEN_EN0,ENABLE);
CSL_FINST(gpioRegs->BINTEN,GPIO_BINTEN_EN1,ENABLE);
CSL_FINST(gpioRegs-> SET_RIS_TRIG01, GPIO_SET_RIS_TRIG01_SETRIS4,RESETVAL);
I also set the pin to input: