but my DM6467T won't boot successfully with the file system over on my Ubuntu/VMware/WindowsXP NFS host.
Please look at the screen capture below from booting and suggest what may be wrong.
For your reference, some IP addresses:
192.168.123.33 = router
192.168.123.18 = Ubuntu/VMware/WindowsXP NFS host
192.168.123.19 = next available IP address from router DHCP client list, that I assign and also gets assigned to EVM
PLEASE NOTE:
1) I believe my router has its own tftp server. This got in the way before of using the dhcp command, and I bypassed it by hard setting some things and using tftpboot.
2) I did a printenv before boot, so you can see what all my environmental variable were beforehand
3) I am particularly concered about the lines after "IP-Config" that show host=...19, bootserver=...33, rootserver=...33, and rootpath=<blank>. I would think these should have been 18,19,19 respectively and "/home/helmutforren/dvdsk/Shared_EVM_FS".
Thanks very much,
Helmut
======================================== Hyperterminal Screen Capture while Booting =====================================
printenv
bootcmd=nboot 0x80700000 0 0x160000; bootm
bootdelay=3
addclk=setenv bootargs ${bootargs} clkref=${clkref}
ethaddr=00:0e:99:02:b7:78
ethact=DaVinci EMAC
ipaddr=192.168.123.19
old_bootargs=mem=112M console=ttyS0,115200n8 root=/dev/hda1 rw ip=off vpif_display.ch2_numbuffers=0 vpif_display.ch3_numbuffers=0
new_bootargs=mem=76M console=ttyS0,115200n8 root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock ip=192.168.123.19 vpif_display.ch2_numbuffers=0 vpif_display.ch3_numbuffers=0
nfshost=192.168.123.18
serverip=192.168.123.18
bootfile=uImage-dm6467t-evm.bin
rootpath=/home/helmutforren/dvdsk/Shared_EVM_FS
baudrate=115200
gateway=192.168.123.33
newdhcp_bootargs=mem=76M console=ttyS0,115200n8 root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock ip=dhcp vpif_display.ch2_numbuffers=0 vpif_display.ch3_numbuffers=0
bootargs=mem=76M console=ttyS0,115200n8 root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock ip=dhcp vpif_display.ch2_numbuffers=0 vpif_display.ch3_numbuffers=0
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2009.08 (Jan 20 2010 - 15:27:59)
Environment size: 1058/16380 bytes
DM6467 EVM > boot
Loading from NAND 128MiB 3,3V 8-bit, offset 0x160000
Image Name: Arago/2.6.31+2.6.32-rc1-r31+gitr
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2061256 Bytes = 2 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Arago/2.6.31+2.6.32-rc1-r31+gitr
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2061256 Bytes = 2 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux...................................................................................................................................... done, booting the kernel.
Linux version 2.6.32-rc2-davinci1 (denis@elrond) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 PREEMPT Mon Jan 11 21:45:54 EST 2010
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DM646x EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci dm6467_rev3.x variant 0x1
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 19304
Kernel command line: mem=76M console=ttyS0,115200n8 root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock ip=dhcp vpif_display.ch2_numbuffers=0 vpif_display.ch3_numbuffers=0
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 76MB = 76MB total
Memory: 72628KB available (3876K code, 335K data, 144K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 246.57 BogoMIPS (lpj=1232896)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 43 gpio irqs
NET: Registered protocol family 16
MUX: Setting register STSOMUX_DISABLE
PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
MUX: Setting register STSIMUX_DISABLE
PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
MUX: Setting register PTSOMUX_DISABLE
PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
MUX: Setting register PTSIMUX_DISABLE
PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
MUX: initialized CIR_UART2
MUX: Setting register CIR_UART2
PINMUX1 (0x00000004) = 0x00000000 -> 0x00000020
MUX: initialized ATAEN
MUX: Setting register ATAEN
PINMUX0 (0x00000000) = 0x00000000 -> 0x00000001
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pcf857x 1-0038: gpios 145..152 on a pcf8574a
pcf857x 1-0038: setup --> -38
vpif vpif: vpif probe success
Switching to clocksource timer0_1
musb_hdrc: version 6.0, pio, peripheral, debug=0
musb_hdrc: USB Peripheral mode controller at fec64000 using PIO, IRQ 13
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 141
io scheduler noop registered
io scheduler anticipatory registered (default)
CIR device registered successfully (Major = 252, Minor = 0)
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c20000 (irq = 40) is a ST16654
console [ttyS0] enabled
serial8250 serial8250.0: unable to register port at index 1 (IO0 MEM1c20400 IRQ41): -22
serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ42): -22
brd: module loaded
loop: module loaded
at24 1-0050: 32768 byte 24c256 EEPROM (writable)
Read MAC addr from EEPROM: 00:0e:99:02:b7:78
Uniform Multi-Platform E-IDE driver
ide-gd driver 1.18
ide0: MMIO-DMA
hda: TOSHIBA MK4032GAX, ATA DISK drive
hda: UDMA/100 mode selected
ide0 at 0xfec661f0-0xfec661f7,0xfec663f6 on irq 22
hda: max request size: 512KiB
hda: 78140160 sectors (40007 MB), CHS=16383/255/63
hda: cache flushes supported
hda: hda1 hda2
NAND device: Manufacturer ID: 0x20, Chip ID: 0xf1 (ST Micro NAND 128MiB 3,3V 8-bit)
Scanning device for bad blocks
Creating 4 MTD partitions on "davinci_nand.0":
0x000000000000-0x000000020000 : "params"
0x000000020000-0x000000160000 : "bootloader"
0x000000160000-0x000000560000 : "kernel"
0x000000560000-0x000008000000 : "filesystem"
davinci_nand davinci_nand.0: controller rev. 2.2
spi_davinci spi_davinci.0: DaVinci SPI driver in EDMA mode
Using RX channel = 17 , TX channel = 16 and event queue = 3
at25 spi0.0: 32 KByte at25640a eeprom, pagesize 64
spi_davinci spi_davinci.0: Controller at 0xfec66800
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
dm9000 Ethernet Driver, V1.31
console [netcon0] enabled
netconsole: network logging started
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbtest
g_ether gadget: using random self ethernet address
g_ether gadget: using random host ethernet address
usb0: MAC e2:b8:50:8f:df:d8
usb0: HOST MAC 0a:f6:72:61:bd:d3
g_ether gadget: Ethernet Gadget, version: Memorial Day 2008
g_ether gadget: g_ether ready
i2c /dev entries driver
Linux video capture interface: v2.00
ths7303 1-002c: chip found @ 0x58 (DaVinci I2C adapter)
ths8200 1-0020: chip found @ 0x40 (DaVinci I2C adapter)
ths7353 1-002e: chip found @ 0x5c (DaVinci I2C adapter)
vpif_capture vpif_capture: registered sub device ths7353
tvp7002 1-005d: tvp7002 1-005d decoder driver registered !!
vpif_capture vpif_capture: registered sub device tvp7002
vpif_capture vpif_capture: DM646x VPIF Capture driver initialized
watchdog watchdog: heartbeat 60 sec
usbcore: registered new interface driver usbhid
usbhid: v2.6:USB HID core driver
Advanced Linux Sound Architecture Driver Version 1.0.21.
No device for DAI tlv320aic3x
asoc: tlv320aic3x <-> davinci-i2s mapping ok
asoc: DIT <-> davinci-dit mapping ok
ALSA device list:
#0: DaVinci DM6467 EVM (tlv320aic3x)
TCP cubic registered
NET: Registered protocol family 17
Clocks: disable unused uart1
Clocks: disable unused emac
Clocks: disable unused timer1
emac-mii: probed
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
eth0: attached PHY driver [ET1011C] (mii_bus:phy_addr=1:01, id=282f013)
Sending DHCP requests ..
PHY: 1:01 - Link is Up - 1000/Full
., OK
IP-Config: Got DHCP answer from 192.168.123.33, my address is 192.168.123.19
IP-Config: Complete:
device=eth0, addr=192.168.123.19, mask=255.255.255.0, gw=192.168.123.33,
host=192.168.123.19, domain=domain.invalid, nis-domain=(none),
bootserver=192.168.123.33, rootserver=192.168.123.33, rootpath=
Looking up port of RPC 100003/2 on 192.168.123.33
rpcbind: server 192.168.123.33 not responding, timed out
Root-NFS: Unable to get nfsd port number from server, using default
Looking up port of RPC 100005/1 on 192.168.123.33
rpcbind: server 192.168.123.33 not responding, timed out
Root-NFS: Unable to get mountd port number from server, using default
Root-NFS: Server returned error -5 while mounting /tftpboot/$(nfshost):$(rootpath)
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option; here are the available partitions:
0300 39070080 hda driver: ide-gd
0301 27342598 hda1
0302 11727450 hda2
1f00 128 mtdblock0 (driver?)
1f01 1280 mtdblock1 (driver?)
1f02 4096 mtdblock2 (driver?)
1f03 125568 mtdblock3 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Backtrace:
[<c00307d0>] (dump_backtrace+0x0/0x114) from [<c030af14>] (dump_stack+0x18/0x1c)
r7:00008000 r6:c3013000 r5:c0026808 r4:c041e850
[<c030aefc>] (dump_stack+0x0/0x1c) from [<c030af6c>] (panic+0x54/0x124)
[<c030af18>] (panic+0x0/0x124) from [<c0008fbc>] (mount_block_root+0x1e0/0x220)
r3:00000001 r2:c3029e98 r1:c3029f60 r0:c0395ead
[<c0008ddc>] (mount_block_root+0x0/0x220) from [<c00090c0>] (mount_root+0xc4/0xfc)
r8:00000000 r7:00000000 r6:00000000 r5:00000000 r4:00200000
[<c0008ffc>] (mount_root+0x0/0xfc) from [<c0009268>] (prepare_namespace+0x170/0x1c8)
r5:c0026808 r4:c041e340
[<c00090f8>] (prepare_namespace+0x0/0x1c8) from [<c00084bc>] (kernel_init+0xe4/0x118)
r5:00000000 r4:c041e100
[<c00083d8>] (kernel_init+0x0/0x118) from [<c0045704>] (do_exit+0x0/0x684)
r5:00000000 r4:00000000