Hi, I got the following error when booting the Wince BSP for logic AM3517 exp board. I did not change any of the default BSP settings, only changes are in the Wince applications, any idea what might going wrong?
Init HW: controller RST
SDCARD: reqested speed 1000000, actual speed 1000000
SDHC: command response timeout CTO!
MMC::MMCCommandResponse: MMCSendCommand error, command = 8
MMC::MMCCommandResponse: Command Response Error
SDCARD: reqested speed 25000000, actual speed 19200000
BL_IMAGE_TYPE_BIN
Download file information:
-----------------------------------------------------------
[0]: Address=0xc0002000 Length=0x013b71c4 Save=0x80002000
-----------------------------------------------------------
Download file type: 6
Invalid flash address/length