Hi,
We intend to use GPIOs 4,5,36 and 38 on dm6467T over git linux v2.6.32. We are using
gpio_request(gpioOut, NULL);
gpio_direction_output(gpioOut , 1);
while(!(__gpio_get_value(gpioIn)));
gpio_set_value(gpioOut, 0);
msleep(800);
gpio_set_value(gpioOut, 1);
Here gpioIn can be GPIO-04 or GPIO-05 and gpioOut is GPIO-36 or GPIO-38 on DM6467T .
We are only able to read GPIO-04 and GPIO-05 levels correctly but we are uable to set the levels on GPIO-36 and GPIO-38.
Please let me know if GPIO initializations are taking place correctly in GIT linux 2.6.32. Any pointers or references in how we can set the GPIO levels under git.
Regards