This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2P-ACD: Ethernet Camera interface with SoC

Part Number: TDA2P-ACD

Dear TI Team,

We are planning to use a 1.3Mpxl cameras with standard H.264  communication format.

Camera Specs are given below

Kindly help us to resolve this query.

Is it possible to interface 6 Ethernet cameras to this SoC, since only 2 ports are available?

If possible how it will interface and what will be the bandwidth requirement?

In 6 Cameras 4 of them are for Surround View System application, which is always ON.

The other 2 ethernet cameras for Forward collission assistance and driver drwosiness detection.

Feature

Specification

Imagesensor(entry/high)

OnSemiAS0143/

OnSemiAR0143

SoC(high)

BCM 89103/7

Operationaltemp.range

-40ºC ~ +85ºC

Waterresistance

IP6K9K (lens side)

ViewAngle(entry/high)

H-FoV: 195

V-FoV: 147

Resolution

1,3Mpx

Dynamicrange

Off the shelf : 96dB

Sensor capacity : 120dB

Sensitivity

> 6V/lux*sec

PowerConsumption

1,2W-2,0W @ 9-16V

LensDiameter

17mm

Videoformat

H264

Connectiontype

Custom Connector

Dims (HxLxD+conn) (mm)

25x27x35