This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VMXEVM: Access SPI interface on evaluation board

Part Number: TDA4VMXEVM

Hello,

we are using the J7x common processor board together with the J721EX SOMG01EVM and would like to use a SPI interface to connect to another board.

Is this interface somewhere on the board accessible? It looks like the standard pin mux and pinout only uses SPI interfaces for flash memory as far as I can see.

If the processor board and SOM supports the external SPI interface, how about the software support (Linux/TI-RTOS)?

Thank you,

Lukas