Part Number: AM5728
Hi
I'd like to confirm if the specific LCDs are available with AM5728.
So, I'd like to send detailed information about LCDs via e-mail.
Please give me feedback if someone is signed to this topic.
Thanks and Best regards,
HaTa.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5728
Hi
I'd like to confirm if the specific LCDs are available with AM5728.
So, I'd like to send detailed information about LCDs via e-mail.
Please give me feedback if someone is signed to this topic.
Thanks and Best regards,
HaTa.
Hi,
Details about available display connections on AM572x devices can be found in:
- Sections 4.4.2, 4.4.3, 7.7, and 7.8 of the AM572x Datasheet Rev. F.
- Section 11 of the AM572x TRM Rev. L.
Hi Biser
I sent the details information about LCD panels offline.
Please confirm it.
Thanks and Best regards,
HaTa.
Hi,
Type 1: Probably supported, but I don't know if the serial interface is required or not. If it's required this display will not be supported directly by our SDK.
Type 2: Not supported. There is no MIPI-DSI interface on AM572x devices.
Type 3: Supported.
Type 4: Not supported.
Hi,
>Type 1: Probably supported, but I don't know if the serial interface is required or not. If it's required this display will not be supported directly by our SDK.
If it's required only parallel then if's supported by SDK?
Thanks and Best regards,
HaTa.