This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 USB 2.0 high speed mode



SPRS586–JUNE 2009 page172  or   SPRS590–JUNE 2009 page 164 :

USB 2.0 peripheral at speeds high speed (HS: 480 Mb/s - C6747 only) and full speed (FS: 12 Mb/s)

USB 2.0 host at speeds HS, FS, and low speed (LS: 1.5 Mb/s)

 

SPRS586B–JUNE 2009–REVISED AUGUST 2010   page 199   or  SPRS590B–JUNE 2009–REVISED AUGUST 2010  page  191  :

USB 2.0 peripheral at speeds high speed (HS: 480 Mb/s) and full speed (FS: 12 Mb/s)

USB 2.0 host at speeds HS, FS, and low speed (LS: 1.5 Mb/s)

 

I may see  2.0 , 1.1 and 1.0 silicon revisions.

1. For what silicon revisins is     " HS: 480 Mb/s - C6747 only  "  ?

2. Is   for host mode    " HS: 480 Mb/s - C6747 only " ?

Alex.

 

  • Alex,

    >>1. For what silicon revisins is     " HS: 480 Mb/s - C6747 only  "  ?

    As for as I know 480Mb/s speed is true for all C674x platform. 

     

    >>2. Is   for host mode    " HS: 480 Mb/s - C6747 only " ?

    This is not for host mode. As mentioned in document it's for peripheral mode.

     

    Regards,
    Ajay