This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

80W BLDC Motor Drive

Hello,

We are working on a new project. Ultimately, we are looking to develop an 80-100W BLDC motor drive system with 370V avg bus voltage including:

  • - Processor with working code
  • - AC-mains supply for motor bus
  • - 3-phase power stage
  • - SMPS for analog and logic circuits
  • - Motor feedback signal conditioning
  • - Speed range requirement is 0.6 to 3600 RPM with 0.1% regulation.
  • - Ideally has scalability up to higher powers (possibly up to a 750W motor)

For the motor drive portion, do you have any product recommendations? 

Best,
Adam