This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2P-ACD: Stream camera feed from the board to PC

Part Number: TDA2P-ACD

I want to stream camera feed from the board to PC.

 

I am trying to run following usecases after selecting AR143 camera from settings. (ISS Usecase “1: 1CH ISS capture + ISS ISP + ISS LDC+VTNF + Display” works fine)

Vision SDK Usecases -> 7: Network RX/TX Usecases

       -> 3: 1CH VIP Capture + Network TX

       AND

       -> 4: 1CH VIP Capture + Encode + Network TX (TDA2x ONLY)

I see below assertion in both the cases.

[IPU1-0]   372.109101 s: Chains: Using TCP/IP

[IPU1-0]   372.113493 s: CAPTURE: Create in progress !!!

[IPU1-0]   372.113707 s: CAPTURE: VIP1 Slice0 PortA capture mode is [ 8-bit] !!!

[IPU1-0]   372.113829 s: captdrv/src/vpsdrv_capturePriv.c @ Line 266:

[IPU1-0]   372.114012 s: Invalid number of streams(0) - Supported max streams 8

[IPU1-0]   372.114103 s: Assertion @ Line: 559 in captureLink_drv.c: pInst->captureVipHandle != NULL : failed !!!

[IPU1-0]   372.114561 s: Assertion @ Line: 559 in captureLink_drv.c: pInst->captureVipHandle != NULL : failed !!!

 

I see from the source code that FVID2_create is failed.

Attached gmake_showconfig_22Jan2020.txt and TDA2P-RTOS-Boot-log-camera-selection-stream-assertion_25Jan2020.txt

[IPU1-0]    372.114561 s:  Assertion @ Line: 559 in captureLink_drv.c: pInst->captureVipHandle != NULL : failed !!!
▒
 TDA2Px SBL Boot

 DPLL Configuration Completed

 Clock Domain Configuration Completed

 Module Enable Configuration Completed

 TI EVM PAD Config Completed

 TDA2Px DDR Configuration

 DDR Config Completed

 App Image Download Begins

 SD Boot - file open completed successfully

 MPU CPU0 Image Load Completed

 IPU1 CPU0 Image Load Completed

 IPU1 CPU1 Image Load Completed

 IPU2 CPU0 and CPU1 Image Load Completed

 DSP1 Image Load Completed

 DSP2 Image Load Completed

 EVE1 Image Load Completed

 EVE2 Image Load Completed

 App Image Download Completed

 Putting MPU CPU1 in Off mode

 EVE MMU configuration completed

 EVE MMU configuration completed

*****************************************************************

 PMCCNTR counts once every 64 clock cycles, multiple by 64 to get actual CPU cycles

 SBL Initial Config Cycles - 118114  (10.7 ms)
 SOC Init Cycles - 170546  (14.55 ms)
 DDR Config Clock Cycles - 89689  (7.65 ms)
 App Image Load Cycles - 277535614  (23683.3 ms)
 Slave Core Bootup Cycles - 130558  (11.14 ms)
 SBL Boot-up Cycles - 278045577  (23726.55 ms)
 Time at which SBL started IPU1_0 - 788132  (24051.87 ms)
*****************************************************************

 Jumping to MPU CPU0 App
[IPU1-0]     24.044348 s:  ***** IPU1_0 Firmware build time 10:13:14 Jan 15 2020
[IPU1-0]     24.044531 s:  *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
[IPU1-0]     24.127188 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
[IPU1-0]     24.127371 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
[IPU1-0]     24.127493 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
[IPU1-0]     24.127584 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
[IPU1-0]     24.127706 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
[IPU1-0]     24.127798 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
[IPU1-0]     24.127920 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
[IPU1-0]     24.129659 s:  *** UTILS: CPU MHz = 20 Mhz ***
[IPU1-0]     24.129811 s:  SYSTEM: System Common Init in progress !!!
[IPU1-0]     24.141767 s:  UTILS: CIO: Init Done !!!
[IPU1-0]     24.141889 s:  SYSTEM: IPC init in progress !!!
[IPU1-0]     24.141950 s:  SYSTEM: Notify init done !!!
[IPU1-0]     24.143750 s:  SYSTEM: MsgQ init done !!!
[IPU1-0]     24.144573 s:  SYSTEM: Work Queue init done !!!
[IPU1-0]     24.144665 s:  SYSTEM: IPC init DONE !!!
[IPU1-0]     24.148600 s:  SYSTEM: System Common Init Done !!!
[IPU1-0]     24.148691 s:  SYSTEM: System Init in progress !!!
[IPU1-0]     24.148783 s:  SYSTEM: BSP Common Init in progress !!!
[IPU1-0]     24.148844 s:  SYSTEM: BSP Common Init Done !!!
[IPU1-0]     24.148905 s:  SYSTEM: BSP Platform Init in progress !!!
[IPU1-0]     24.149027 s:  SYSTEM: BSP Platform Init Done !!!
[IPU1-0]     24.149118 s:  SYSTEM: FVID2 Init in progress !!!
[IPU1-0]     24.149271 s:  SYSTEM: FVID2 Init Done !!!
[IPU1-0]     24.149393 s:  SYSTEM: VPS Init in progress !!!
[IPU1-0]     24.149484 s:  SYSTEM: VPDMA Descriptor Memory Address translation ENABLED [0xa0000000 -> 0x80000000]
[IPU1-0]     24.152961 s: *** VPDMA Firmware Loading... ***
[IPU1-0]     24.153083 s: VPDMA Firmware Address = 0x9fd1b5c0
[IPU1-0]     24.153175 s: VPDMA Load Address     = 0x4897d004
[IPU1-0]     24.153266 s: VPDMA Firmware Version = 0x4d0001b8
[IPU1-0]     24.153358 s: VPDMA List Busy Status = 0x00000000
[IPU1-0]     24.153480 s: *** VPDMA Firmware Load Success ***
[IPU1-0]     24.153876 s: *** VPDMA Firmware Loading... ***
[IPU1-0]     24.153968 s: VPDMA Firmware Address = 0x9fd1b5c0
[IPU1-0]     24.154059 s: VPDMA Load Address     = 0x4899d004
[IPU1-0]     24.154181 s: VPDMA Firmware Version = 0x4d0001b8
[IPU1-0]     24.154273 s: VPDMA List Busy Status = 0x00000000
[IPU1-0]     24.154334 s: *** VPDMA Firmware Load Success ***
[IPU1-0]     24.154791 s: *** VPDMA Firmware Loading... ***
[IPU1-0]     24.154883 s: VPDMA Firmware Address = 0x9fd1b5c0
[IPU1-0]     24.154974 s: VPDMA Load Address     = 0x489dd004
[IPU1-0]     24.155096 s: VPDMA Firmware Version = 0x4d0001b8
[IPU1-0]     24.155157 s: VPDMA List Busy Status = 0x00000000
[IPU1-0]     24.155249 s: *** VPDMA Firmware Load Success ***
[IPU1-0]     24.230921 s:  SYSTEM: VPS Init Done !!!
[IPU1-0]     24.231836 s:  UTILS: DMA: HWI Create for INT34 !!!
[IPU1-0]     24.232050 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
[IPU1-0]     24.232141 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 254232 B (248 KB)
[IPU1-0]     24.232294 s:  SYSTEM: Heap = SR_OCMC              @ 0x00000000, Total size = 0 B (0 KB), Free size = 0 B (0 KB)
[IPU1-0]     24.232507 s:  SYSTEM: Heap = SR_DDR_CACHED        @ 0x88583000, Total size = 368037888 B (350 MB), Free size = 368037888 B (350 MB)
[IPU1-0]     24.232751 s:  SYSTEM: Heap = SR_DDR_NON_CACHED    @ 0xbfc00000, Total size = 127872 B (0 MB), Free size = 106368 B (0 MB)
[IPU1-0]     24.232934 s:  SYSTEM: Initializing Links !!!
[IPU1-0]     24.533916 s:  SYSTEM: Initializing Links ... DONE !!!
[IPU1-0]     24.587384 s:  BOARD: Board Init in progress !!!
[IPU1-0]     24.587842 s:  BOARD: Board Init Done !!!
[IPU1-0]     24.601598 s:
[IPU1-0]     24.601659 s:  Vision SDK Version    : [REL_VISION_SDK_03_08_00_00]
[IPU1-0]     24.601750 s:  FVID2 Version         : [FVID_02_01_00_01]
[IPU1-0]     24.601811 s:  BSP Version           : [PDK_01_10_04__xx]
[IPU1-0]     24.601872 s:  Platform              : [EVM]
[IPU1-0]     24.601964 s:  SOC                   : [TDA2PX]
[IPU1-0]     24.602025 s:  SOC Revision          : [ES1.0]
[IPU1-0]     24.602086 s:  Board Detected        : [Vision]
[IPU1-0]     24.607637 s:  EEPROM Base Board Name: [DRA76/7xP,TDA2P]
[IPU1-0]     24.607728 s:  Base Board Revision   : [REV A]
[IPU1-0]     24.609040 s:  Daughter Card Revision: [REV D]
[IPU1-0]     24.609131 s:
[IPU1-0]     24.612853 s:  SYSTEM: UART: INTERRUPT Mode is Selected
[IPU1-1]     24.060300 s:  ***** IPU1_1 Firmware build time 10:08:42 Jan 15 2020
[IPU1-1]     24.060483 s:  *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
[IPU1-1]     24.129475 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
[IPU1-1]     24.129689 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
[IPU1-1]     24.129811 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
[IPU1-1]     24.129964 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
[IPU1-1]     24.130055 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
[IPU1-1]     24.130177 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
[IPU1-1]     24.130269 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
[IPU1-1]     24.132190 s:  SYSTEM: System Common Init in progress !!!
[IPU1-1]     24.133288 s:  UTILS: CIO: Init Done !!!
[IPU1-1]     24.133410 s:  SYSTEM: IPC init in progress !!!
[IPU1-1]     24.133502 s:  SYSTEM: Notify init done !!!
[IPU1-1]     24.135271 s:  SYSTEM: MsgQ init done !!!
[IPU1-1]     24.136064 s:  SYSTEM: Work Queue init done !!!
[IPU1-1]     24.136155 s:  SYSTEM: IPC init DONE !!!
[IPU1-1]     24.139754 s:  SYSTEM: System Common Init Done !!!
[IPU1-1]     24.139876 s:  SYSTEM: System IPU1_1 Init in progress !!!
[IPU1-1]     24.140700 s:  UTILS: DMA: HWI Create for INT25 !!!
[IPU1-1]     24.140913 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
[IPU1-1]     24.141035 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 655360 B (640 KB), Free size = 647600 B (632 KB)
[IPU1-1]     24.141188 s:  SYSTEM: Initializing Links !!!
[IPU1-1]     24.252577 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM7 ####
[IPU1-1]     24.252729 s:  SYSTEM: Initializing Links ... DONE !!!
[IPU1-1]     24.252790 s:  SYSTEM: System IPU1_1 Init Done !!!
[HOST  ]     24.121606 s:  ***** A15_0 Firmware build time 10:11:39 Jan 15 2020
[HOST  ]     24.121637 s:  *** SYSTEM: CPU Frequency <ORG = 750000000 Hz>, <NEW = 750000000 Hz>
[HOST  ]     24.128103 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
[HOST  ]     24.128133 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
[HOST  ]     24.128164 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
[HOST  ]     24.128164 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
[HOST  ]     24.128164 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
[HOST  ]     24.128194 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
[HOST  ]     24.128194 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
[HOST  ]     24.130818 s:  SYSTEM: System Common Init in progress !!!
[HOST  ]     24.130848 s:  SYSTEM: IPC init in progress !!!
[HOST  ]     24.130848 s:  SYSTEM: Notify init done !!!
[HOST  ]     24.130879 s:  SYSTEM: MsgQ init done !!!
[HOST  ]     24.130909 s:  SYSTEM: Work Queue init done !!!
[HOST  ]     24.130940 s:  SYSTEM: IPC init DONE !!!
[HOST  ]     24.131489 s:  SYSTEM: System Common Init Done !!!
[HOST  ]     24.131519 s:  SYSTEM: System A15 Init in progress !!!
[HOST  ]     24.131550 s:  UTILS: DMA: HWI Create for INT66 !!!
[HOST  ]     24.131580 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
[HOST  ]     24.131580 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 6291456 B (6144 KB), Free size = 6248624 B (6102 KB)
[HOST  ]     24.131611 s:  SYSTEM: Initializing Links !!!
[HOST  ]     24.133929 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC1 ####
[HOST  ]     24.133990 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC2 ####
[HOST  ]     24.134081 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC3 ####
[HOST  ]     24.134142 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM0 ####
[HOST  ]     24.134203 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM1 ####
[HOST  ]     24.134295 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM2 ####
[HOST  ]     24.134356 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM3 ####
[HOST  ]     24.134447 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM4 ####
[HOST  ]     24.134508 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM5 ####
[HOST  ]     24.134600 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM6 ####
[HOST  ]     24.134691 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM7 ####
[HOST  ]     24.134691 s:  SYSTEM: Initializing Links ... DONE !!!
[HOST  ]     24.134752 s:  SYSTEM: System A15 Init Done !!!
[HOST  ]     24.428536 s:  NSP GMAC: PHY 2 Found on MAC Port 0
[HOST  ]     24.430854 s:  NSP GMAC: PHY 3 Found on MAC Port 1
[DSP1  ]     24.106081 s:  ***** DSP1 Firmware build time 10:02:32 Jan 15 2020
[DSP1  ]     24.106142 s:  *** SYSTEM: CPU Frequency <ORG = 600000000 Hz>, <NEW = 600000000 Hz>
[DSP1  ]     24.131641 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
[DSP1  ]     24.131702 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
[DSP1  ]     24.131733 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
[DSP1  ]     24.131763 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
[DSP1  ]     24.131794 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
[DSP1  ]     24.131824 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
[DSP1  ]     24.131855 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
[DSP1  ]     24.132007 s:  *** UTILS: CPU MHz = 20 Mhz ***
[DSP1  ]     24.132068 s:  SYSTEM: System Common Init in progress !!!
[DSP1  ]     24.132251 s:  UTILS: CIO: Init Done !!!
[DSP1  ]     24.132282 s:  SYSTEM: IPC init in progress !!!
[DSP1  ]     24.132312 s:  SYSTEM: Notify init done !!!
[DSP1  ]     24.132465 s:  SYSTEM: MsgQ init done !!!
[DSP1  ]     24.132587 s:  SYSTEM: Work Queue init done !!!
[DSP1  ]     24.132617 s:  SYSTEM: IPC init DONE !!!
[DSP1  ]     24.133349 s:  SYSTEM: System Common Init Done !!!
[DSP1  ]     24.133380 s:  SYSTEM: System DSP Init in progress !!!
[DSP1  ]     24.133563 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
[DSP1  ]     24.133624 s:  SYSTEM: Heap = LOCAL_L2             @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
[DSP1  ]     24.133685 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 524288 B (512 KB), Free size = 516616 B (504 KB)
[DSP1  ]     24.133715 s:  SYSTEM: Initializing Links !!!
[DSP1  ]     24.141798 s:  SYSTEM: Initializing Links ... DONE !!!
[DSP1  ]     24.141859 s: lz4CompDecomp Init
[DSP1  ]     24.141859 s:  SYSTEM: System DSP Init Done !!!
[DSP1  ]     24.548221 s:  SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after boot !!!
[DSP1  ]     24.548252 s:  SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after update by APP !!!
[DSP2  ]     24.106081 s: ***** DSP2 Firmware build time 10:05:49 Jan 15 2020
[DSP2  ]     24.106142 s:  *** SYSTEM: CPU Frequency <ORG = 600000000 Hz>, <NEW = 600000000 Hz>
[DSP2  ]     24.132831 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
[DSP2  ]     24.132892 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
[DSP2  ]     24.132922 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
[DSP2  ]     24.132953 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
[DSP2  ]     24.132983 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
[DSP2  ]     24.133014 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
[DSP2  ]     24.133044 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
[DSP2  ]     24.133197 s:  *** UTILS: CPU MHz = 20 Mhz ***
[DSP2  ]     24.133227 s:  SYSTEM: System Common Init in progress !!!
[DSP2  ]     24.133441 s:  UTILS: CIO: Init Done !!!
[DSP2  ]     24.133471 s:  SYSTEM: IPC init in progress !!!
[DSP2  ]     24.133502 s:  SYSTEM: Notify init done !!!
[DSP2  ]     24.133624 s:  SYSTEM: MsgQ init done !!!
[DSP2  ]     24.133746 s:  SYSTEM: Work Queue init done !!!
[DSP2  ]     24.133776 s:  SYSTEM: IPC init DONE !!!
[DSP2  ]     24.134539 s:  SYSTEM: System Common Init Done !!!
[DSP2  ]     24.134569 s:  SYSTEM: System DSP Init in progress !!!
[DSP2  ]     24.134783 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
[DSP2  ]     24.134813 s:  SYSTEM: Heap = LOCAL_L2             @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
[DSP2  ]     24.134874 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 524288 B (512 KB), Free size = 516616 B (504 KB)
[DSP2  ]     24.134905 s:  SYSTEM: Initializing Links !!!
[DSP2  ]     24.142835 s:  SYSTEM: Initializing Links ... DONE !!!
[DSP2  ]     24.142896 s: lz4CompDecomp Init
[DSP2  ]     24.142896 s:  SYSTEM: System DSP Init Done !!!
[DSP2  ]     24.550204 s:  SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after boot !!!
[DSP2  ]     24.550234 s:  SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after update by APP !!!
[EVE1  ]     24.057616 s:  ***** EVE Firmware build time 09:52:02 Jan 15 2020
[EVE1  ]     24.059385 s:  *** SYSTEM: CPU Frequency <ORG = 267500000 Hz>, <NEW = 267500000 Hz>
[EVE1  ]     24.135362 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
[EVE1  ]     24.136887 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
[EVE1  ]     24.138321 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
[EVE1  ]     24.139663 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
[EVE1  ]     24.141035 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
[EVE1  ]     24.142377 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
[EVE1  ]     24.143658 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
[EVE1  ]     24.145885 s:  SYSTEM: System Common Init in progress !!!
[EVE1  ]     24.147928 s:  UTILS: CIO: Init Done !!!
[EVE1  ]     24.148844 s:  SYSTEM: IPC init in progress !!!
[EVE1  ]     24.149789 s:  SYSTEM: Notify init done !!!
[EVE1  ]     24.151619 s:  SYSTEM: MsgQ init done !!!
[EVE1  ]     24.153022 s:  SYSTEM: Work Queue init done !!!
[EVE1  ]     24.153968 s:  SYSTEM: IPC init DONE !!!
[EVE1  ]     24.166534 s:  SYSTEM: System Common Init Done !!!
[EVE1  ]     24.167510 s:  SYSTEM: System EVE Init in progress !!!
[EVE1  ]     24.168944 s:  UTILS: DMA: HWI Create for INT8 !!!
[EVE1  ]     24.170103 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
[EVE1  ]     24.171353 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
[EVE1  ]     24.173549 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 254408 B (248 KB)
[EVE1  ]     24.175623 s:  SYSTEM: Initializing Links !!!
[EVE1  ]     24.263161 s:  SYSTEM: Initializing Links ... DONE !!!
[EVE1  ]     24.264198 s:  SYSTEM: System EVE Init Done !!!
[EVE2  ]     24.061123 s:  ***** EVE Firmware build time 09:59:12 Jan 15 2020
[EVE2  ]     24.062801 s:  *** SYSTEM: CPU Frequency <ORG = 267500000 Hz>, <NEW = 267500000 Hz>
[EVE2  ]     24.135362 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
[EVE2  ]     24.136887 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
[EVE2  ]     24.138321 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
[EVE2  ]     24.139663 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
[EVE2  ]     24.141035 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
[EVE2  ]     24.142408 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
[EVE2  ]     24.143689 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
[EVE2  ]     24.145915 s:  SYSTEM: System Common Init in progress !!!
[EVE2  ]     24.147959 s:  UTILS: CIO: Init Done !!!
[EVE2  ]     24.148874 s:  SYSTEM: IPC init in progress !!!
[EVE2  ]     24.149820 s:  SYSTEM: Notify init done !!!
[EVE2  ]     24.151650 s:  SYSTEM: MsgQ init done !!!
[EVE2  ]     24.153053 s:  SYSTEM: Work Queue init done !!!
[EVE2  ]     24.153998 s:  SYSTEM: IPC init DONE !!!
[EVE2  ]     24.166595 s:  SYSTEM: System Common Init Done !!!
[EVE2  ]     24.167541 s:  SYSTEM: System EVE Init in progress !!!
[EVE2  ]     24.169005 s:  UTILS: DMA: HWI Create for INT8 !!!
[EVE2  ]     24.170133 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
[EVE2  ]     24.171384 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
[EVE2  ]     24.173580 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 254408 B (248 KB)
[EVE2  ]     24.175654 s:  SYSTEM: Initializing Links !!!
[EVE2  ]     24.263130 s:  SYSTEM: Initializing Links ... DONE !!!
[EVE2  ]     24.264167 s:  SYSTEM: System EVE Init Done !!!
[IPU2  ]     24.042152 s:  ***** IPU2 Firmware build time 10:16:53 Jan 15 2020
[IPU2  ]     24.042365 s:  *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
[IPU2  ]     24.130635 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
[IPU2  ]     24.130787 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
[IPU2  ]     24.130909 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
[IPU2  ]     24.131001 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
[IPU2  ]     24.131123 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
[IPU2  ]     24.131245 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
[IPU2  ]     24.131336 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
[IPU2  ]     24.134051 s:  SYSTEM: System Common Init in progress !!!
[IPU2  ]     24.135271 s:  UTILS: CIO: Init Done !!!
[IPU2  ]     24.135423 s:  SYSTEM: IPC init in progress !!!
[IPU2  ]     24.135515 s:  SYSTEM: Notify init done !!!
[IPU2  ]     24.137314 s:  SYSTEM: MsgQ init done !!!
[IPU2  ]     24.138077 s:  SYSTEM: Work Queue init done !!!
[IPU2  ]     24.138168 s:  SYSTEM: IPC init DONE !!!
[IPU2  ]     24.143323 s:  SYSTEM: System Common Init Done !!!
[IPU2  ]     24.143475 s:  SYSTEM: System IPU2 Init in progress !!!
[IPU2  ]     24.144238 s:  UTILS: DMA: HWI Create for INT25 !!!
[IPU2  ]     24.144512 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
[IPU2  ]     24.144604 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 254336 B (248 KB)
[IPU2  ]     24.144756 s:  SYSTEM: Initializing Links !!!
[IPU2  ]     24.248551 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC1 ####
[IPU2  ]     24.251235 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC2 ####
[IPU2  ]     24.253949 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC3 ####
[IPU2  ]     24.256847 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM0 ####
[IPU2  ]     24.259684 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM1 ####
[IPU2  ]     24.262612 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM2 ####
[IPU2  ]     24.265509 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM3 ####
[IPU2  ]     24.268315 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM4 ####
[IPU2  ]     24.271182 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM5 ####
[IPU2  ]     24.274049 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM6 ####
[IPU2  ]     24.276947 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM7 ####
[IPU2  ]     24.277069 s:  SYSTEM: Initializing Links ... DONE !!!
[IPU2  ]     24.277130 s:  SYSTEM: System IPU2 Init Done !!!
[IPU1-0]     25.646281 s:  UTILS_PRCM_STATS: INA226 Setup Failed. Check if INA226 is connected on I2C3 Lines
[IPU1-0]     25.651192 s:  QSPI Init Started
[IPU1-0]     25.651467 s:  MID - 1
[IPU1-0]     25.651528 s:  DID - 18
[IPU1-0]     25.651558 s:  QSPI Init Completed Sucessfully
[IPU1-0]     25.666839 s:
[IPU1-0]     25.666900 s:  Current System Settings,
[IPU1-0]     25.666961 s:  ========================
[IPU1-0]     25.667022 s:  Display Type   : HDMI 1920x1080 @ 60fps
[IPU1-0]     25.667083 s:  Capture Source : Sensor OV10635 1280x720  @ 30fps - VIP, YUV422
[IPU1-0]     25.667175 s:  My IP address for interface 1 : 0.0.0.0
[IPU1-0]     25.667236 s:  My IP address for interface 2 : 0.0.0.0
[IPU1-0]     25.667297 s:  ISS Settings   : LDC=[OFF] VTNF=[OFF] WDR=[OFF]
[IPU1-0]     25.667388 s:
[IPU1-0]     25.667449 s:  ============
[IPU1-0]     25.667510 s:  Usecase Menu
[IPU1-0]     25.667541 s:  ============
[IPU1-0]     25.667602 s:
[IPU1-0]
[IPU1-0]  Vision SDK Usecases,
[IPU1-0]  --------------------
[IPU1-0]  1: Single Camera Usecases
[IPU1-0]  2: Multi-Camera LVDS Usecases
[IPU1-0]  3: AVB RX Usecases, (TDA2x & TDA2Ex ONLY)
[IPU1-0]  4: Dual Display Usecases, (TDA2x EVM ONLY)
[IPU1-0]  5: ISS Usecases, (TDA3x ONLY)
[IPU1-0]  6: TDA2x Stereo Usecases
[IPU1-0]  7: Network RX/TX Usecases
[IPU1-0]  9: RADAR Usecases
[IPU1-0]  a: Miscellaneous test's
[IPU1-0]  f: TIDL Usecase
[IPU1-0]  g: Camera Radar Combo Usecases
[IPU1-0]
[IPU1-0]  s: System Settings
[IPU1-0]
[IPU1-0]  x: Exit
[IPU1-0]
[IPU1-0]  Enter Choice:
[IPU1-0]
[HOST  ]     26.029219 s:  NDK: Link Status: 100Mb/s Full Duplex on PHY 2
[HOST  ]     29.134386 s:  NETWORK_CTRL: Starting Server (port=5000) !!!
[HOST  ]     29.134417 s:  NETWORK_CTRL: Starting Server ... DONE (port=5000) !!!
[IPU1-0]     50.425150 s:
[IPU1-0]     50.425211 s:
[IPU1-0]
[IPU1-0]  ===============
[IPU1-0]  System Settings
[IPU1-0]  ===============
[IPU1-0]
[IPU1-0]  1: Display Settings
[IPU1-0]  2: Capture Settings
[IPU1-0]  3: ISS Settings (TDA3x ONLY)
[IPU1-0]  4: Enable Charging via USB2 Port (TDA2x EVM ONLY)
[IPU1-0]  5: Print PRCM Statistics
[IPU1-0]  6: Show Memory/CPU/DDR BW usage
[IPU1-0]  7: Calibration Settings
[IPU1-0]
[IPU1-0]  x: Exit
[IPU1-0]
[IPU1-0]  Enter Choice:
[IPU1-0]
[IPU1-0]     50.425486 s:
[IPU1-0]     52.297535 s:
[IPU1-0]
[IPU1-0]  ==============
[IPU1-0]  Capture Source
[IPU1-0]  ==============
[IPU1-0]
[IPU1-0]  1: OV10635 Sensor 720P30
[IPU1-0]  2: HDMI Capture 1080P60 (Not Supported in TDA2x/TDA2Ex Multi-serdes board)
[IPU1-0]  3: OV10640 Sensor 720P30 - CSI2 (TDA3x ONLY)
[IPU1-0]  4: OV10640 Sensor 720P30 - Parallel (TDA3x ONLY)
[IPU1-0]  5: AR0132  Sensor 720P60 - Parallel (TDA3x ONLY)
[IPU1-0]  6: AR0140  Sensor 720P60 - Parallel (TDA3x ONLY)
[IPU1-0]  7: IMX224  Sensor 1280x960 - CSI2 (TDA3x ONLY)
[IPU1-0]  8: AR0140  Sensor for SV - TIDA00262 (TDA3x ONLY)
[IPU1-0]  9: OV10640 Sensor for SV - IMI (TDA3x ONLY)
[IPU1-0]  a: OV10635 Sensor for Mosaic Display - SAT0088/OV10635 (TDA2PX, TDA2EX & TDA3x)
[IPU1-0]  b: OV2775 Sensor 1080p30 (TDA3x ONLY)
[IPU1-0]  c: AR143 MARS Camera (TDA3x ONLY)
[IPU1-0]  d: Skip Sensor configuration
[IPU1-0]  e: OV2775 Sensor 1080p30 - TIDA001130
[IPU1-0]  f: IMX390 Sensor 1080p30 - D3
[IPU1-0]  g: OV10640 Sensor + OV490 ISP - IMI
[IPU1-0]  h: AR0233 RCCB UB953 - MARS
[IPU1-0]  i: OV2311 UB953 - Leopard Imaging
[IPU1-0]  j: AR0239 RGBIR UB953 - MARS
[IPU1-0]
[IPU1-0]  x: Exit
[IPU1-0]
[IPU1-0]  Enter Choice:
[IPU1-0]
[IPU1-0]     52.298328 s:
[IPU1-0]     55.784786 s:  MARS AR0143 Selected
[IPU1-0]     55.785060 s:
[IPU1-0]     55.785091 s:  Current System Settings,
[IPU1-0]     55.785152 s:  ========================
[IPU1-0]     55.785243 s:  Display Type   : HDMI 1920x1080 @ 60fps
[IPU1-0]     55.785304 s:  Capture Source : Sensor AR0143 MARS 1280x800 @ 30fps - ISS CSI2, Bayer (TDA3x EVM ONLY)
[IPU1-0]     55.785426 s:  My IP address for interface 1 : 192.168.1.3
[IPU1-0]     55.785487 s:  My IP address for interface 2 : 0.0.0.0
[IPU1-0]     55.785548 s:  ISS Settings   : LDC=[OFF] VTNF=[OFF] WDR=[OFF]
[IPU1-0]     55.785640 s:
[IPU1-0]     55.785670 s:  ============
[IPU1-0]     55.785701 s:  Usecase Menu
[IPU1-0]     55.785762 s:  ============
[IPU1-0]     55.785792 s:
[IPU1-0]
[IPU1-0]  Vision SDK Usecases,
[IPU1-0]  --------------------
[IPU1-0]  1: Single Camera Usecases
[IPU1-0]  2: Multi-Camera LVDS Usecases
[IPU1-0]  3: AVB RX Usecases, (TDA2x & TDA2Ex ONLY)
[IPU1-0]  4: Dual Display Usecases, (TDA2x EVM ONLY)
[IPU1-0]  5: ISS Usecases, (TDA3x ONLY)
[IPU1-0]  6: TDA2x Stereo Usecases
[IPU1-0]  7: Network RX/TX Usecases
[IPU1-0]  9: RADAR Usecases
[IPU1-0]  a: Miscellaneous test's
[IPU1-0]  f: TIDL Usecase
[IPU1-0]  g: Camera Radar Combo Usecases
[IPU1-0]
[IPU1-0]  s: System Settings
[IPU1-0]
[IPU1-0]  x: Exit
[IPU1-0]
[IPU1-0]  Enter Choice:
[IPU1-0]
[IPU1-0]     61.590373 s:
[IPU1-0]     61.590526 s:
[IPU1-0]
[IPU1-0]  Select use-case,
[IPU1-0]  ----------------
[IPU1-0]  1: Network RX + Display
[IPU1-0]  2: Network RX + Decode + Display (TDA2x ONLY)
[IPU1-0]  3: 1CH VIP Capture + Network TX
[IPU1-0]  4: 1CH VIP Capture + Encode + Network TX (TDA2x ONLY)
[IPU1-0]  5: 4CH VIP Capture + Network TX
[IPU1-0]
[IPU1-0]  x: Exit
[IPU1-0]
[IPU1-0]  Enter Choice:
[IPU1-0]
[IPU1-0]     66.717013 s: Chains: Using TCP/IP
[IPU1-0]     66.720917 s:  CAPTURE: Create in progress !!!
[IPU1-0]     66.721130 s:  CAPTURE: VIP1 Slice0 PortA capture mode is [ 8-bit] !!!
[IPU1-0]     66.721252 s: captdrv/src/vpsdrv_capturePriv.c @ Line 266:
[IPU1-0]     66.721344 s: Invalid number of streams(0) - Supported max streams 8
[IPU1-0]     66.721435 s:  Assertion @ Line: 559 in captureLink_drv.c: pInst->captureVipHandle != NULL : failed !!!
[IPU1-0]     66.721954 s:  Assertion @ Line: 559 in captureLink_drv.c: pInst->captureVipHandle != NULL : failed !!!

Microsoft Windows [Version 10.0.10240]
(c) 2015 Microsoft Corporation. All rights reserved.

C:\Users\sgandiga>cd C:\PROCESSOR_SDK_VISION_03_08_00_00\vision_sdk\build

C:\PROCESSOR_SDK_VISION_03_08_00_00\vision_sdk\build>
C:\PROCESSOR_SDK_VISION_03_08_00_00\vision_sdk\build>gmake showconfig
gmake -C C:/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/configs -f build_makeconfig.mk showconfig
gmake[1]: Entering directory `C:/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/configs'
#
# Build Config is [ tda2px_evm_bios_all ]
# Build Config file is @ C:/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/configs/tda2px_evm_bios_all/cfg.mk
# Build Config .h file is @ C:/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/links_fw/include/config/apps/tda2px_evm_bios_all/system_cfg.h
# Build CPUs is @ ipu1_0 ipu1_1 ipu2 a15_0 dsp1 dsp2 eve1 eve2
#
# CPUs included in application,
# PROC_IPU1_0_INCLUDE=yes
# PROC_IPU1_1_INCLUDE=yes
# PROC_IPU2_INCLUDE=yes
# PROC_DSP1_INCLUDE=yes
# PROC_DSP2_INCLUDE=yes
# PROC_EVE1_INCLUDE=yes
# PROC_EVE2_INCLUDE=yes
# PROC_EVE3_INCLUDE=no
# PROC_EVE4_INCLUDE=no
# PROC_A15_0_INCLUDE=yes
#
# Platform config,
# VSDK_BOARD_TYPE=TDA2PX_EVM [options: TDA2XX_EVM TDA2EX_EVM TDA3XX_EVM TDA3XX_RVP TDA2XX_RVP]
# PLATFORM=tda2px-evm
# DUAL_A15_SMP_BIOS=no
# IPU1_SMP_BIOS=no
# DDR_MEM=DDR_MEM_512M [options: DDR_MEM_128M DDR_MEM_512M DDR_MEM_1024M]
# EMIFMODE=SINGLE_EMIF_512MB [options: SINGLE_EMIF_512MB SINGLE_EMIF_1GB ref build_pdk.mk]
# NDK_PROC_TO_USE=a15_0 [options: a15_0 ipu1_0 ipu1_1 ipu2 none]
# NSP_TFDTP_INCLUDE=no [options: yes no]
# TDA2EX_ETHSRV_BOARD=no [options: yes no]
# FATFS_PROC_TO_USE=ipu1_0 [options: ipu1_0 none]
# RADAR_BOARD=none [options: TDA3XX_AR12_ALPS TDA3XX_AR12_VIB_DAB_BOOSTER TDA3XX_RADAR_RVP none]
#
# Build config,
# BUILD_OS=Windows_NT [options: Windows_NT Linux]
# BUILD_DEPENDENCY_ALWAYS=no
# BUILD_ALGORITHMS=no
# BUILD_INFOADAS=no
# PROFILE=release [options: debug release]
# KW_BUILD=no
# CPLUSPLUS_BUILD=no
# IPU_PRIMARY_CORE=ipu1_0 [options: ipu1_0 ipu2]
# IPU_SECONDARY_CORE=ipu2 [options: ipu1_0 ipu2]
# A15_TARGET_OS=Bios [options: Bios Linux Qnx]
# BSP_STW_PACKAGE_SELECT=all [options: all vps-iss-dss-only vps-vip-vpe]
#
# Safety Module config,
# RTI_INCLUDE=no
# ECC_FFI_INCLUDE=no
# DCC_ESM_INCLUDE=no
#
# Video Module config,
# IVAHD_INCLUDE=yes
# VPE_INCLUDE=yes
# CAL_INCLUDE=yes
# ISS_INCLUDE=yes
# ISS_ENABLE_DEBUG_TAPS=no
# WDR_LDC_INCLUDE=no
# DSS_INCLUDE=yes
#
# Open Compute config,
# OPENCL_INCLUDE=no
# TARGET_ROOTDIR=C:/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/src/rtos/opencl
# ENABLE_OPENCV=no
# ENABLE_OPENCV_TESTS=no
# OPENVX_INCLUDE=no
#
# Log config,
# ENABLE_UART_LOG=yes
# ENABLE_NETWORK_LOG=no
# ENABLE_CCS_LOG=no
# CIO_REDIRECT=yes
#
# IPC config,
# WORKQ_INCLUDE=yes
# IPC_LIB_INCLUDE=no
#
# AUTOSAR_APP=no
#
# Surround View config,
# SRV_FAST_BOOT_INCLUDE=no
#
# Other Module config,
# AVB_INCLUDE=no
# DCAN_INCLUDE=no
# RADAR_ONLY=no
# RADAR_STUDIO=no
# CPU_IDLE_ENABLED=yes
# FAST_BOOT_INCLUDE=no
# DATA_VIS_INCLUDE=no
# HS_DEVICE=no
# ULTRASONIC_INCLUDE=no
# PGA450=
# PGA460=
# ENABLE_ALL_DEPTH=
#
# Linux config,
# DEFAULT_UBOOT_CONFIG=dra7xx_evm_vision_config
# DEFAULT_KERNEL_CONFIG=ti_sdk_dra7x_release_defconfig
# DEFAULT_DTB=dra7-evm-infoadas.dtb
# CMEM_INCLUDE=no
# IPUMM_INCLUDE=no
# IPU1_EVELOADER_INCLUDE=no
# ROBUST_RVC_INCLUDE=no
# BUILD_ADAM_CAR=no
#
# Alg plugins included in build,
# ALG_autocalibration ALG_clr ALG_deWarp ALG_dmaSwMs ALG_vpeSwMs ALG_edgedetection ALG_framecopy ALG_lanedetection ALG_objectdetection ALG_safe_framecopy ALG_sceneobstruction ALG_sfm ALG_sparseopticalflow ALG_subframecopy ALG_surroundview ALG_tidl ALG_rgbirprocess ALG_rgbirmux ALG_radarprocess ALG_iss_aewb
#
# Use-cases included in build,
# UC_iss_capture_isp_simcop_display UC_iss_mult_capture_isp_2d_3d_sv_tda3x UC_iss_mult_capture_isp_dewarp_3dsv_tda3xx UC_iss_mult_capture_isp_simcop_sv_tda3xx UC_iss_multi_inst_capture_display UC_srv_calibration UC_lvds_vip_multi_cam_view UC_lvds_vip_sv_standalone UC_network_rx_tx UC_null_src_dec_display UC_null_src_display UC_saveDisFrame UC_vip_single_cam_analytics2 UC_vip_single_cam_edge_detection UC_vip_single_cam_frame_copy UC_vip_single_cam_frame_copy_safety UC_vip_single_cam_lane_detection UC_vip_single_cam_object_detection2 UC_vip_single_cam_sfm UC_vip_single_cam_sparse_optical_flow UC_vip_single_cam_subframe_copy UC_vip_single_cam_tlr UC_vip_single_cam_view UC_vip_single_cam_view_encdec UC_csi2_cal_multi_cam_view UC_camera_radar_capture_display UC_tidl_OD_radar_process_display UC_iss_capture_rgbir_isp_display UC_radar_objectdetect_display
#
gmake -s -fbuild_makeconfig.mk check_cpu_include
gmake[2]: Entering directory `C:/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/configs'
#
# CPUs that are NOT required but included in config [ tda2px_evm_bios_all ],
#
# WARNING: IPU1_1 can be excluded from application
# WARNING: IPU2 can be excluded from application
#
# CPUs that are required but not included in config [ tda2px_evm_bios_all ],
#
#
# Edit C:/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/configs/tda2px_evm_bios_all/cfg.mk to include or exclude CPUs in an application
#
gmake[2]: Leaving directory `C:/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/configs'
gmake[1]: Leaving directory `C:/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/configs'

C:\PROCESSOR_SDK_VISION_03_08_00_00\vision_sdk\build>

  • Hi Sandeep,

    If i remember correctly, AR0143 sensor is supported for ISS usecases, but not for VIP usecases. I think OV10635 sensor is supported for VIP usecases.

    Rgds,

    Brijesh

  • Hi Brijesh,

    Thanks for the info.

    Could you please suggest how to expand/modify this use case to allow any capture source (AR143 camera in my case, selected under “System Settings/Capture source”)?

    Thanks,
    Sandeep

  • Hi Sandeep,

    But how is your sensor connected to the TDA device? Is it over parallel interface or CSI? If it is parallel, is it connected over VIP or ISS? 

    Based on where it is connected, we need to use either ISS capture link or VIP capture link. Rest of the pipeline you could reuse from the existing usecase. 

    Regards,

    Brijesh

  • Hi Brijesh,

    This is what I see in the log "Capture Source : Sensor AR0143 MARS 1280x800 @ 30fps - ISS CSI2, Bayer (TDA3x EVM ONLY)". I understand the camera is connected over ISS-CSI2, so we are looking at merging ISS capture, encode and Network usecases into one.

    I am wondering if you already have this  working, if yes, we would like to get it, if not, please suggest us the parts in the existing use cases on how we should modify them.  

    Thanks,

    Sandeep

  • Hi Sandeep,

    I dont think we have a usecase. You could use single camera ISS usecase and merge it with encoder link at the ISP output.

    Please note that you need to use ISP, because this sensor outputs RAW data, that needs to be converted into YUV420 using ISP. 

    Regards,

    Brijesh