I do not yet have a successful build of the complete package for a TDA4 system.
I started with the Vision Apps Users Guide page and it implied more instructions on screen than I saw.
It was not quite obvious that after I ran the install.bin executable that I would then need to run the sdk-install.sh script. I would think that one would invoke the other and only one iteration would be required.
However the issue remains that the RTOS_Auto package and the processor Linux j7 evm package do not know where each other is.
this is giving me errors out of the make program, some of which were corrected by setting TI_RTOS_PATH and then adding a symbolic link to point from the RTOS install path to the subdirectory under packages/ti/build to point to a Rules.make file that seem to be expected in a directory named processor_sdk_rtos_j7_6_01_01_12
It may or may not be the correct Rules.make, file.
I am currently stuck with a message that says recipe for target 'ti-ipc-linux-config' failed: in that it could not execute a cd to a directory of the named target.
It is quite possible that all the issues will cure themselves if there is a "correct" set of directories to install into.
At this time, if have the PSDKLA (Linux applications side) in my home directory ~/ti-processor-sdk-Linux-automotive(…)
And I have the PSDKRA (rtos auto package)e under ~/ti_tools/psdk_rtos_auto_j7(…)
A little direction would be appreciated.
Regards,
- - Scott