Part Number: TMDSIDK437X
Other Parts Discussed in Thread: TIDEP0064, , AM3359, SYSBIOS
We have purchased and received the TMDSIDK437X board with the intention of using it as a Real-Time Ethernet Tracer for the AM3359 ICE SORTE protocol. It came with as SD card, however we cannot read this card because it is not in FAT format. I have reveiwed the TRM "tiducd4 Tracer DOcs,pdf." We ordered is as a TIDEP0064 device. I was expecting this device to boot up with the tracer program installed or on the SD card. It appears that it does not. Do we need to build the projects and load them somehow onto the device?
I did download all of the required software tools and attampted to compile it. It appears that the RTE-Tracer_PRU_ICSS project did build, but the RTE_TRACER_ARM_NDX did not. It failed with the following error:
"This project does not contain a buildable RTSC Configuration (.cfg) file. In order for it to build, this project must contain one RTSC Configuration file that is not excluded from build. RTE_Tracer_ARM_NDK RTE_Tracer_ARM_NDK " If I include the file nimu_idk.cfg I then get the following errors:
ti.sysbios.BIOS: incompatible assignment to kernelHeapSection : ".kernel_heap" .xdchelp /RTE_Tracer_ARM_NDK line 926 C/C++ Problem
Is there an already built file to load on the board to run it as a tracer?
Thank you for your help,
Drew Tkac