Part Number: AM3358
Other Parts Discussed in Thread: AM3352, TPS65910
hello,
we have dev. an am3358 based custom board with ref. design of sitara kit
there is only one change in our board there is two ddr3 ram and we have configure board.c for the same
at boot time we are getting log such as
U-Boot SPL 2019.01-g1ebdbc7d8b-dirty (Jan 29 2020 - 18:41:33 +0530)
Trying to boot from MMC1
U-Boot 2019.01-g1ebdbc7d8b-dirty (Jan 29 2020 - 18:41:33 +0530)
========================================
**************** AAROHI ****************
========================================
CPU123 : AM335X123-GP rev 2.1
=====> Inside sys_info.c
Model: TI AM335x EVM
DRAM: 1 GiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0
Loading Environment from FAT... OK
Net: Could not get PHY for ethernet@4a100000: addr 0
Warning: ethernet@4a100000 MAC addresses don't match:
Address in ROM is 04:79:b7:03:11:19
Address in environment is 04:79:b7:03:41:f4
eth0: ethernet@4a100000
Warning: usb_ether MAC addresses don't match:
Address in ROM is de:ad:be:ef:00:01
Address in environment is 04:79:b7:03:41:f6
, eth1: usb_ether
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr **
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
4227584 bytes read in 274 ms (14.7 MiB/s)
37166 bytes read in 4 ms (8.9 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to bdf2b000, end bdf3712d ... OK
Starting kernel ...
after that cpu hangs
here are some boot time cmd test results
=> bdinfo
arch_number = 0x00000e05
boot_params = 0x80000100
DRAM bank = 0x00000000
-> start = 0x80000000
-> size = 0x40000000
baudrate = 115200 bps
TLB addr = 0xbfff0000
relocaddr = 0xbff68000
reloc off = 0x3f768000
irq_sp = 0xbdf398c0
sp start = 0xbdf398b0
Early malloc usage: 1ac / 1000
fdt_blob = 0xbdf398d8
=> iminfo
## Checking Image at 82000000 ...
Unknown image format!
=> mmc info
Device: OMAP SD/MMC
Manufacturer ID: 1b
OEM: 534d
Name: 00000
Bus Speed: 48000000
Mode : SD High Speed (50MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 7.5 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
=>
i am confuse
because due to what reason kernel not coming up ...?