Other Parts Discussed in Thread: OMAP-L137
Hello,
We are using OMAP-L137's USB port in "Device" mode,
in our custom board whenever we Power on the board and connect the
USB to a host(PC), the temperature of the device(OMAP-L137) goes very high
from 60 degC to 80 degC.
The temperature remains same even if the power is removed but USB cable is still connected.
But the temperature goes down if the USB cable is diconnected.
We are investigating if there is any mistake in our USB circuit.
Is this kind of issue related to USB VBUS?
Please let me know if anybody has experienced this kind of issue and
if there are any references.
Thankyou in advance.