This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BEAGLEBK: PTP timestamp issue

Part Number: BEAGLEBK

Hi,

We'd like to use AM335x in our product. We bought a Beaglebone black to test some of its performance. We'd like to implement the one step hardware time stamp linuxptp on it. we have checked the driver and hardware support using ethtool. The timestamping parameters for eth0 is:

Capabilities:

       hardware-transmit     (SOF_TIMESTAMPING_TX_HARDWARE)

       software-transmit     (SOF_TIMESTAMPING_TX_SOFTWARE)

       hardware-receive     (SOF_TIMESTAMPING_RX_HARDWARE)

       software-receive     (SOF_TIMESTAMPING_RX_SOFTWARE)

       software-system-clock (SOF_TIMESTAMPING_SOFTWARE)

       hardware-raw-clock   (SOF_TIMESTAMPING_RAW_HARDWARE)

PTP Hardware Clock: 0

Hardware Transmit Timestamp Modes:

       off                   (HWTSTAMP_TX_OFF)

        on                   (HWTSTAMP_TX_ON)

Hardware Receive Filter Modes:

       none                                    (HWTSTAMP_FILTER_NONE)

       ptpv1-14-event                   (HWTSTAMP_FILTER_PTP_V1-L4_EVENT)

       ptpv2-event                        (HWTSTAMP_FILTER_PTP_V2__EVENT)

 However, when we run:

 ptp4l -2 -i eth0 -m -f /etc/linuxptp.cfg

 We got the following error message:

 selected /dev/ptp0 as PTP clock

driver rejected most general HWTSTAMP filter

ioctl SIOCSHWTSTAMP failed: Numerical result out of range

port 1: INITIALIZING to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)

port 0: INITIALIZING to LISTENING on INIT_COMPLETE

The content of /etc/linuxptp.cfg is:

[global]

twoStepFlag            0

time_stamping         hardware

When we were running ptp4l as two-step hardware stamping, there is no problem. We are very grateful if anybody can tell us what caused this problem. 

Best regards.

Lee