This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/AM3352: Eth0 causes kernel crash

Part Number: AM3352

Tool/software: TI C/C++ Compiler

Hi Champs:

While using the Ethernet Cable plugging on the Router, I did not do anything.

The System will crash like the below log.

Any idea?

SDK is 5.02.

BR Rio

root@am335x-evm:/etc/network# [ 3047.040833] ------------[ cut here ]------------
[ 3047.045580] WARNING: CPU: 0 PID: 0 at net/sched/sch_generic.c:320 dev_watchdog+0x2c0/0x2c4
[ 3047.053898] NETDEV WATCHDOG: eth0 (cpsw): transmit queue 0 timed out
[ 3047.060290] Modules linked in: sha512_generic sha512_arm sha256_generic sha1_generic sha1_arm_neon sha1_arm md5 aes_arm_bs crypto_simd cryptd des_generic cbc xfrm_user xfrm4_tunnel ipcomp xfrm_ipcomp esp4 ah4 af_key xfrm_algo pru_rproc pruss_intc pruss usb_f_acm u_serial usb_f_ecm musb_dsps musb_hdrc phy_am335x phy_generic phy_am335x_control g_multi bc_example(O) usb_f_mass_storage usb_f_rndis u_ether libcomposite udc_core snd_soc_simple_card snd_soc_simple_card_utils pm33xx wkup_m3_ipc wkup_m3_rproc remoteproc omap_aes_driver crypto_engine pvrsrvkm(O) omap_crypto ti_emif_sram omap_sham pruss_soc_bus at24 musb_am335x rtc_omap omap_wdt sch_fq_codel uio_module_drv(O) uio ftdi_sio usbserial usbcore usb_common cryptodev(O)
[ 3047.124775] CPU: 0 PID: 0 Comm: swapper Tainted: G O 4.14.79-gbde58ab01e #10
[ 3047.133001] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 3047.139131] Backtrace:
[ 3047.141649] [<c010b6f0>] (dump_backtrace) from [<c010b9d4>] (show_stack+0x18/0x1c)
[ 3047.149274] r7:00000009 r6:00000000 r5:c0b18dd0 r4:c0d01d00
[ 3047.154992] [<c010b9bc>] (show_stack) from [<c0834688>] (dump_stack+0x24/0x28)
[ 3047.162284] [<c0834664>] (dump_stack) from [<c0128aa8>] (__warn+0xe8/0x100)
[ 3047.169304] [<c01289c0>] (__warn) from [<c0128b00>] (warn_slowpath_fmt+0x40/0x48)
[ 3047.176846] r9:dc1ea000 r8:00000000 r7:ffffe000 r6:c0d15280 r5:00000000 r4:c0b18d94
[ 3047.184651] [<c0128ac4>] (warn_slowpath_fmt) from [<c0735bb0>] (dev_watchdog+0x2c0/0x2c4)
[ 3047.192879] r3:dc1ea000 r2:c0b18d94
[ 3047.196481] r4:dc1ea000
[ 3047.199070] [<c07358f0>] (dev_watchdog) from [<c017f194>] (call_timer_fn.constprop.4+0x30/0xa0)
[ 3047.207831] r8:c07358f0 r7:ffffe000 r6:c07358f0 r5:00000101 r4:ffffe000
[ 3047.214593] [<c017f164>] (call_timer_fn.constprop.4) from [<c017f2f0>] (expire_timers+0xec/0xf4)
[ 3047.223434] r6:c0d152c0 r5:00000000 r4:c0d01dac
[ 3047.228102] [<c017f204>] (expire_timers) from [<c017f3a8>] (run_timer_softirq+0xb0/0x200)
[ 3047.236343] r9:00000101 r8:c0d01da4 r7:c0d152c0 r6:c0d15280 r5:c0d152c0 r4:c0d01da8
[ 3047.244149] [<c017f2f8>] (run_timer_softirq) from [<c01015a4>] (__do_softirq+0xe4/0x274)
[ 3047.252298] r8:c0d50e00 r7:ffffe000 r6:40000001 r5:c0d50e04 r4:00000000
[ 3047.259058] [<c01014c0>] (__do_softirq) from [<c012c494>] (irq_exit+0x120/0x154)
[ 3047.266513] r10:6f69a35b r9:c0d00000 r8:dc008000 r7:00000000 r6:00000000 r5:00000010
[ 3047.274389] r4:c0d4d93c
[ 3047.276960] [<c012c374>] (irq_exit) from [<c0169f98>] (__handle_domain_irq+0x60/0xb0)
[ 3047.284849] [<c0169f38>] (__handle_domain_irq) from [<c0101464>] (omap_intc_handle_irq+0x3c/0x98)
[ 3047.293786] r9:c0d00000 r8:00000001 r7:c0d01ed4 r6:ffffffff r5:00070013 r4:c0d82630
[ 3047.301588] [<c0101428>] (omap_intc_handle_irq) from [<c010c58c>] (__irq_svc+0x6c/0xa8)
[ 3047.309665] Exception stack(0xc0d01ea0 to 0xc0d01ee8)
[ 3047.314772] 1ea0: 00000000 000002c5 05355555 c0d0f800 dc5c0600 ffffe000 000002c5 71c65ba0
[ 3047.323014] 1ec0: 00000001 dc5c0600 6f69a35b c0d01f2c c0d01ef0 c0d01ef0 c065c77c c065c780
[ 3047.331242] 1ee0: 00070013 ffffffff
[ 3047.334759] r5:00070013 r4:c065c780
[ 3047.338393] [<c065c60c>] (cpuidle_enter_state) from [<c065c970>] (cpuidle_enter+0x1c/0x20)
[ 3047.346720] r10:c0d4eeb8 r9:c0d030d0 r8:c0d42e60 r7:c0d030c4 r6:dc5dd000 r5:ffffe000
[ 3047.354619] r4:dc5c0600
[ 3047.357192] [<c065c954>] (cpuidle_enter) from [<c015a9e8>] (call_cpuidle+0x28/0x40)
[ 3047.364907] [<c015a9c0>] (call_cpuidle) from [<c015ac54>] (do_idle+0x168/0x1b4)
[ 3047.372271] [<c015aaec>] (do_idle) from [<c015af58>] (cpu_startup_entry+0x14/0x18)
[ 3047.379900] r10:dcfffbc0 r9:c0c3ba28 r8:c0d50240 r7:c0d03040 r6:ffffffff r5:00000002
[ 3047.387776] r4:c0d0edc4
[ 3047.390352] [<c015af44>] (cpu_startup_entry) from [<c08476a4>] (rest_init+0xb0/0xb4)
[ 3047.398166] [<c08475f4>] (rest_init) from [<c0c00d60>] (start_kernel+0x3b4/0x3c0)
[ 3047.405696] r5:c0d50240 r4:c0d5028c
[ 3047.409311] [<c0c009ac>] (start_kernel) from [<80008078>] (0x80008078)
[ 3047.415880] ---[ end trace b0c3bd6a6aba9e9f ]---