Other Parts Discussed in Thread: TMS320DM6446
hi,
I have a TMS320DM6446 EVM
I have downloaded the SDK files from the http://software-dl.ti.com/dsps/dsps_registered_sw/sdo_sb/targetcontent/dvsdk/mv_dvsdk/v1_30/index.html TI website.
m referring to the sprue66d.pdf (TMS320DM6446 DVEVM v1.30 Getting Started Guide)
1) in section 4.2 (Preparing to Install)
there is a list of files to be downloaded.
❏ mvl_4_0_1_demo_sys_setuplinux.bin
❏ mvl_4_0_1_demo_target_setuplinux.bin
❏ mvl_4_0_1_demo_lsp_setuplinux_#_#_#_#.bin
❏ dvsdk_setuplinux_#_#_#_#.bin
❏ xdc_setuplinux_#_#_#_#.bin
❏ bios_setuplinux_#_#_#_#.bin
❏ TI-C6x-CGT-v#.#.#.#.bin
i got all the files except the last two files which have probably different names as
❏dsp_bios_setuplinux_5_31_08_15.bin
❏TI-C6x-CGTEVAL-v6.0.15.1.bin
so i used these two files install the SDK.
will this cause any problem?
2) section 3.4 (Running the Demos from the Command Line)
i am instructed to run the following commands
Target $ cd /opt/dvsdk/dm6446
Target $ ./loadmodules.sh
when i run them i get the following msg
root@10.42.43.11:/opt/dvsdk/dm6446# ./loadmodules.sh
-bash: ./loadmodules.sh: No such file or directory
root@10.42.43.11:/opt/dvsdk/dm6446# ls
cmemk.ko
root@10.42.43.11:/opt/dvsdk/dm6446#
3) as my board is not manufactured by TI, i considered to build a new kernel and port it throuh the TFTP
section 4.5- Building a New Linux Kernel
To rebuild the Linux Kernel, follow these steps:
1) Log in to your user account (not as root).
2) Set the PLATFORM variable in the Rules.make file as described in
Section 4.6.
3) Use commands like the following to make a local working copy of the
MontaVista Linux Support Package (LSP) in your home directory.
This copy contains the embedded Linux 2.6.10 kernel plus the
DaVinci drivers. If you installed in a location other than /opt/mv_pro_4.0.1, use your location in the cp command.
host $ cd /home/<useracct>
host $ mkdir -p workdir/lsp
host $ cd workdir/lsp
host $ cp -R /opt/mv_pro_4.0.1/montavista/pro/devkit/lsp/ti-davinci .
but i get a permission denied error
cp: cannot create regular file `./ti-davinci/Documentation/video4linux/CARDLIST.bttv': Permission denied
cp: cannot create regular file `./ti-davinci/Documentation/video4linux/API.html': Permission denied
cp: cannot create regular file `./ti-davinci/.mvl_target_cpu': Permission denied
cp: cannot create regular file `./ti-davinci/Makefile': Permission denied
so i tried to change the owner by
[aditya@localhost lsp]$ chmod +x /opt/mv_pro_4.0.1/montavista/pro/devkit/lsp/ti-davinci
chmod: changing permissions of `/opt/mv_pro_4.0.1/montavista/pro/devkit/lsp/ti-davinci': Operation not permitted
so i logged in as root
and executed the cp command ..
4) Use the following commands to configure the kernel using the
DaVinci defaults. Note that CROSS_COMPILE specifies a prefix for
the executables that is used during compilation:
host $ cd ti-davinci/linux-2.6.10_mvl401
host $ make ARCH=arm CROSS_COMPILE=arm_v5t_le- davinci_dm644x_defconfig
[aditya@localhost ~]$ cd /
[aditya@localhost /]$ cd home/aditya/workdir/lsp/
[aditya@localhost lsp]$ cd ti-davinci
[aditya@localhost ti-davinci]$ ls
arch Documentation init lib mm REPORTING-BUGS usr
COPYING drivers ipc localversion mvl_patches scripts
CREDITS fs kernel MAINTAINERS net security
crypto include ktools Makefile README sound
[aditya@localhost ti-davinci]$
and i cannot see any linux-2.6.10_mvl401 folder in it...