This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3XEVM: TDA3XEVM does not work

Part Number: TDA3XEVM

TDA3XEVM Board  was purchased from spectra digital.

input 12V power. using power supply.

current consumption was about 300ma.

DIP SW mode was set to nor or qspi mode.

After Power on , not work..

1.

using  term term , setting  serial port at UART3 , 1152000,  

but  no letter on screen.

2.  don't connect  using  black hawk usb560v2 system trace

  1) ccs  and   black hawk usb560v2 system trace  connect board . at mipi60 

  2)  message "power loss "

i  bought two evm board but the same . ..