tda3x evm board was purchased from spectra digital. I entered 12v power using the power supply. The current consumes about 300 ma. Using tera term, I selected 115200 and uart third serial port for monitoring. Dip sw is set to qspi or nor mode.
1)
after power on No letters appear after power on.
2) I used blackhawk's usb560 v2 system trace and ccs to connect to the mipi60 slot. If i will connect, message "power loss" I bought two evm boards and they all work the same.