I want to use the external JTAG of the J7 EVM with ARM DStream for which I need the RDDI files.
I tried gathering the board information using ARM DS-5 configure tool in order to write a debug script to be used with DStream but didn't succeed. Between the JTAG chain and my connector, the ICEPick module, which is the JTAG route controller, needs to be configured. And I did not find any information to do this.