Hi,
few weeks ago I received theC6A816x/AM389x EVM board.
I followed what is written in documentation, I used the SD card within the pack, I configure the board to boot from SD,
but I haven't got any result.
I when I boot from the SD CARD, with the sd supplied, after few moments, I can see the DDR turn on, the clock begin to run at 400 Mhz,
and begin the activity on the RAS and CAS signals. This actitvity seem be refresh cycles of memory, I didn't see any activity similar to read and write on memory.
I cannot see any string appearing on the serial port.
I tried to download the first stage boot from TFTP and I got the same result, same activity on SDRAM after the download.
Anyone has the same problem on the board?
Best regards,
Giacomo.