This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power sequence without AVS

Guru 10570 points


Hello,
For simple power designing, I would not like to use AVS for core voltage(CVDD).
But, the datasheet describes that "Implementation of SmartReflex AVS is required for proper device operation."(SPRS680.pdf : P132)

- Can I use constant power supply for CVDD?
If yes,
- Can I bring the following sequences(1-V AVS and 1-V constant) together in one?

1. 3.3 V
2. 1-V AVS
3. 1-V Constant
4. 1.8 V
5. 1.5 V
6. 0.9 V

Thank you in advance.
Best regards,
RY