Part Number: TDA4VMXEVM
Hello,
I've got the TDA4VMxEVM, which consists of SOM and Common Processor Board (CP).
I would like to test the SPI functionality, therefore I search a way to connect easily the Common Processor Board to an external SPI slave. I need CLK, MOSI, MISO, and CS for this.
Is there any test header on the CP which I can use for this? Like the J20 SPI1 Header on the AM6548IDK?
Or do I need to buy an additional expansion board?
Best regards,
Thomas